Part Number: TPS25820 My customer need IEC-62368 certification data which has been described on the TPS25820 datasheet. Please kindly support it ?
Best Regards, Hironori Yoshimura
Part Number: TUSB1142 Other Parts Discussed in Thread: TPS25820 , Tool/software: The TUSB1142 design uses the Flip signal from a TPS25820 to switch the SuperSpeed signals from a USB Type C connector. We are not able to get SuperSpeed to work at all.
Part Number: TPS25820 Other Parts Discussed in Thread: TPS65987D Dear team,
I wonder if TPS25820 could get power supply from Type C Vbus 5V, not use its own power supply, let OUT as NC, only use CC pin to detection?
Thanks.
Best regards,
Sammi
Part Number: TPS25820 Dear team,
Customer has not detect well when inserted USB. Would you kindly help check schematic and give some suggestion?
I could see that the input capacitor is not enough and the power supply of Vin and POL is different. Not sure…
Hi Thomas ,
I dont see 200ohm on TPS25820 and TPS25821 Evaluation Modules (Rev. A) .
Can you please share the document you are referring to.
Thanks ,
Shubha
Part Number: TPS25820 Other Parts Discussed in Thread: TPS25810 Greetings,
I'm looking for an integrated to charge with USB-C up to 5W.
I would like to do a USB-C charger up to 5W.
I used TPs25820 but it source up to 7,5W.
Do you have some integrated…
Part Number: TUSB1142 Other Parts Discussed in Thread: TPS25820 , TUSB1044 , TUSB321 , TUSB322 Hello, I have to implement a board which takes USB3 from a host into a USB3 type-C connector and drive in some way the USB3 signal towards another type-C connector…
Part Number: TUSB1142 Other Parts Discussed in Thread: TPS25820 ,
Our TUSB1142 design uses the Flip signal from a TPS25820 to switch the superspeed signals from a Type C connector. We are not able to get Superspeed to work at all. Once the Flip signal…
Part Number: TPS25820 Hi, my customer uses TPS25820 and wants to be able to really break the circuit, in case of a overload situation.
They use it in at a USB C Audio Accessory Port.
Can the "current limiting function" do a really hard break, or it there…
Part Number: TPS25820 Hi,
in the datasheet, there is Ios specified for a certain resistor value Rref:
Rref is 10 Ohms which displays a threshold of 1.72 A.
Can there be a different value for Rref selected and with this the threshold shifted?
Kind…