Part Number: TPS25833-Q1 Other Parts Discussed in Thread: TPS25831Q1EVM-062 Tool/software: Hi! I'm currently using TPS25833-Q1 for a USB charger design and making some tests with the TPS25831Q1EVM-062 Ev. board. It is clear that the TPS2583X-Q1 family…
Part Number: TPS25833-Q1 Tool/software: Hi team,
If I continue to use the unit in the following settings under overcurrent conditions, will there be any malfunctions or other problems? I understand that operating in this mode will cause a voltage drop…
Part Number: TPS25833-Q1 Tool/software: Hi team,
When the current limit is set to 2A and a device compatible with APPLE's Divider (D+:2.7, D-:2.7V) is connected and 2.4A current is tried to flow, or when the device recognizes 5V/3A on the CC pin and…
Part Number: TPS25833-Q1 Tool/software: Hi
Below is my customer's schematics, it is now switchinng at 300KHz.
From the datasheet efficiency curve, for 300KHz, 3A output, it shows greater than 90% efficiency.
However for 300KHz 3A output, my customer…
Part Number: TPS25833-Q1 Other Parts Discussed in Thread: TPS25831-Q1 , Good morning,
I kindly ask for the differences between the TPS25831-Q1 model and the TPS25833-Q1 model
looking at the datasheets I don't find any differences, but I think something…
Part Number: TPS25833-Q1 Tool/software: Hi Team,
When a 1M or 1.5M cable is added to VBUS (Type-C connector), the output voltage will become lower. How should I set IMON? Or are there other solutions?
Vin:7~16V
Vout:5V
Iout:3A
IMON Pin R9…
Part Number: TPS25833-Q1 Tool/software: Hi Team,
At present, when the load is increased to 3 amps, the output voltage is too high. Please give me some suggest.