Hi ,
The TPS25850-Q1 internal FET VDS max rating is 30V. The 40V just a short time period transient withstand not for long time normal operation.
If your application is need support 36V for long time, I suggest you choose TPS25831-Q1 or TPS25833-Q1 single…
Hi Sir,
Pls. find my comment as below:
1. The current requirement specification is USB A-type connector specification.
In this case, what is the maximum current support?--> TPS25840-Q1 can support 3.5A output charge.
2. Should I connect the TPS25840…
Hi,
The TPS25840-Q1 will not reset the OUT VBUS during model change (SDP/CDP).
If the phone need to re-plug in to identify this is a SDP or CDP port.
The TPS25840-Q1 have only SDP/CDP mode but don't have DCP mode.
If you want high current charge for…
Hello Dani,
Yes, you can choose the TPS25833-Q1 for your application.
The external Mosfet just need have enough margin for the 1.5A continous current is OK.
Hi Aham,
It is constant voltage buck.
The TPS25832-Q1 is focus on data communication, it don't have the DCP function but it can configure to CDP mode which mean can charge up to 1.5A in type A and 3A in type C.
The TPS25833-Q1 have the DCP function…
Part Number: TPS25830-Q1 Other Parts Discussed in Thread: TPS25833-Q1 Hi,
Can tps25830-q1/tps25833-q1 be used like mpq4482-c in the figure below?That is,DM and DP communicate with host directly without passing through USB switch inside the chip. The reason…