Part Number: TPS3420 Hi expert,
Customer is asking for solution which is similar like TPS3420 but will need to keep low or high status for output and toggle status to high or low at next pulse generated by push button. Do we have solution could support…
Part Number: TPS3420 Hello,
I've observed a strange behavior on my design.
The TPS3420 is used as shown below :
When the two inputs are low, sometimes it works and output becomes low, and sometimes output remains high.
Do you have any suggestion…
Part Number: TPS3420 Hi sir/madam,
I am trying to find the CAD package for TPS3420 , but have not been able to find it in the Altium Vault or TI online. Could you please point me to it or send it?
Best Regards,
Other Parts Discussed in Thread: TPS3420 Hi,
My customer use TPS3420, and have some question. They only use one botton, so PB2 always connect to GND.
1. Should PB1 need pull high resistor?Or can use GPIO to control the high/low level? (VIH ≥ 0.85 V, and…
Part Number: TPS3421 Other Parts Discussed in Thread: TPS3420 , TPS3899 , , TPS3820
Hi team,
my customer want this function but the delay and reset pulse duration option are not much to choose,
they want Trst=10ms ,
do we have other solution that can fit…
Part Number: TPS3421 Other Parts Discussed in Thread: TPS3422 , TPS3420 Hello,
My customer is evaluating the TPS3421 device on the EVM and they are seeing that if voltage is present on either PB pin when VCC is not present, the VCC rails powers up to a…
Other Parts Discussed in Thread: TPS3420 Good morning,
I am looking for a smd chip with latching circuit integrated, for switches (push button for example, max current 500mA).
The latching circuit when connected to the push button should:
- From OFF…
Ben,
Both TPS3431 and TPS3851 have a reset timeout period (tRST from the timing diagram in datasheet figure 1) so WDO will automatically de-assert without WDI changing. In my application, this would mean that the charger would be re-enabled after tRST…
Part Number: TPS3422 Other Parts Discussed in Thread: TPS3421 , , TPS3420 Dear Team,
The customer is using LTC2955.
Do we have roadmap with AEC-Q100?
BR
Kevin