Part Number: TPS3422 Hello,
Instead of a reset push button, is there a way I can use the TPS3422 to reset my battery powered device by removing USB power for <10 seconds then reapplying power? I would also like for no reset signal to be sent when the…
Part Number: TPS3422 Other Parts Discussed in Thread: TPS3421 The part which label shows TPS3422EGDRYT, but after decapsulation it marks TPS3421, pls help to confirm the difference, thx.
Part Number: TPS3421 Other Parts Discussed in Thread: TPS3422 , Hello TI experts,
my customer is right before in mass production, but they cannot get TPS3422 because of the delivery issue.
I found TPS3421, and also I found it can replace from TPS3422,…
Part Number: TPS3422 Other Parts Discussed in Thread: TPS65287 Hey there,
I would like to realise a button debouncer with TPS3422 or similar device.
The goal is to take a push button as an input device to enable and disable a buck converter.
I don't…
Part Number: TPS3422 Other Parts Discussed in Thread: SN74LVC1G123 Hi Team,
For our application, we want to use TPS3422 with 0second delay. Can we connect TS to VCC to achieve this?
There is a note in datasheet, that this option is only for factory setting…
Hi Binyamin,
Thanks for your question! I just want to clarify the behavior.
The Reset will be asserting as long as the voltage at Sense pin is below than threshold. CTS (sense delay) and CTR (reset delay) are the adjustable time delays, which delays the…
Part Number: TPS3422 Hi team,
Could you help provide a RESET IC solution for pulse output as below?
And after pulse out will go back to high?
Even IC is no action, RESET output is high.
We saw the TPS3422 has the function but not for 12V rail.
The pulse…
This circuit does not have a one-second delay. (The hold time is only 5 ns and refers to something different.)
Your specification is unclear. What should happen to the output when the button is pressed? What should happen to the output when the button…