Part Number: TPS56921 Hello,
My customer is designing with TPS56921 referring EVM desgin. Let me confirm below design for below usage condition.
Vin: 12V, Vout: 1.0V, Iout: 1A (max), Fsw: 400kHz
1. Can 1.5uH of L1 inductance be used?
2. Can below components…
Part Number: TPS56921 Other Parts Discussed in Thread: TPS56C215 , TPS56C230 , TPS56920 HI
we have this Micro Semi 5A part LX7178-01CSP-TR in our design that has Constant Frequency Hysteretic Control with extremely fast or near-instantaneous load/line step…
Part Number: TPS56921 We need to operate this at the maximum switching frequency of 1.6 Mhz as set by a resistor. There is no option in the web bench to change the frequency. It is set at 532 Khz or similar. Can this feature be implemented in the web…
Other Parts Discussed in Thread: TPS56921 , USB2ANY Hi, I am using TPS56921 right now. I found that the GUI for TPS56921 is USB2ANY GUI. How about the USB bridge? Is it also a USB2ANY Bridge? I had a USB Interface Adapter (TI 2006). Is this one OK to communicate…
Other Parts Discussed in Thread: TPS54821 , TPS56921 , TPS54620 , TPS54020 Hello,
When will WEBENCH support the TPS56921 ?
Are there any alternatives (e.g. Excel)?
Thank you,
Chris
Other Parts Discussed in Thread: TPS56921 Hello,
We have customize board based on TI DM8148. We have TPS56921 as "12V TO 1.1V BUCK CONVERTER" for processor's voltage and according to TPS56921 datasheet, we can configure its output voltage using I2C register…
Hi Chris,
I would suggest you post your request of TPS56921 in a seperate thread. WEBENCH related question can be posted to WEBENCH forum:
http://e2e.ti.com/support/development_tools/webench_design_center/f/235.aspx
Regards,
Na