Part Number: TPS62111 We plan to use the TPS62111MRSAREP in addition to the TPS62111RSAR. The main differences are TPS62111RSAR TPS62111MRSAREP Temperature range - 40 .. 85°C to -55 ... 125°C Tolerance output voltage +-3% to +-7%. Now the question arises…
Part Number: TPS62111-EP Other Parts Discussed in Thread: TPS62111 Hi Experts,
Good day!
May I know how to calculate or what is the thermal resistance (junction-to-case, junction to board, etc.) of this enhanced buck-converter product in RSA package…
Part Number: TPS62111 Ripple more than 40mVp-p @ 5Khz with 6mA load @ 3.3V.
as im using for the 4-20mA loop it should be less than 10mVp-p
please suggest some solution.
Other Parts Discussed in Thread: TPS62111 , TPS62160 , TPS62140 We have a board design using a TPS62111 3.3 volt regulator driven by a user inserted battery. The PG pin out of the TPS 62111 is used to hold off a Master Reset circuit for a few seconds…
You might post in the high-rel forum for the -EP version but for the catalog version, the upper range of the abs max for the SW pin is simply due to the body diode of the high side FET. Applying a voltage at SW greater than 0.3V above the voltage at the…
If DVDD3318_A, DVDD3318_B, or DVDD3318_C exceed STATIC 1.8V by more than 2V, can this damage the chip, or just cause a malfunction? This will not be a problem on power-up, but on power-down the decay of the supplies depends on how much power is drawn…
Part Number: TPS62110-EP Other Parts Discussed in Thread: TPS62110 , TPS62111 , TPS62110-Q1 ,
Hi Team,
Two questions from a customer:
1. The EP version of TPS62110 supports a higher temp range than the standard and Q1 versions for which it has a…