Part Number: TPS62111 We plan to use the TPS62111MRSAREP in addition to the TPS62111RSAR. The main differences are TPS62111RSAR TPS62111MRSAREP Temperature range - 40 .. 85°C to -55 ... 125°C…
Part Number: TPS62111-EP Other Parts Discussed in Thread: TPS62111 Hi Experts,
Good day!
May I know how to calculate or what is the thermal resistance (junction-to-case, junction to board, etc.) of this enhanced buck-converter product in RSA package -…
Koteswar,
In PFM mode the TPS62111 operates in a semi-hysteretic manner. It switches at the normal switching frequency until Vout is 0.8% above nominal, then does not switch until Vout falls to the nominal value. This cannot be adjusted.
In PFM mode,…
Part Number: TPS62113 Other Parts Discussed in Thread: TPS62110 , , TPS62111 , TPS62112 Hi team,
Customer want to use tps62113 replace TPS62110 and in their design, LBI connect to GND. Will it work? when use tps62113 and LBI isn't used, should LBI connect…
Part Number: TPS62110-EP Other Parts Discussed in Thread: TPS62110 , TPS62111 , TPS62110-Q1 ,
Hi Team,
Two questions from a customer:
1. The EP version of TPS62110 supports a higher temp range than the standard and Q1 versions for which it has a higher feedback…
Other Parts Discussed in Thread: TPS62111 , TPS62160 , TPS62140 We have a board design using a TPS62111 3.3 volt regulator driven by a user inserted battery. The PG pin out of the TPS 62111 is used to hold off a Master Reset circuit for a few seconds to ensure…
You might post in the high-rel forum for the -EP version but for the catalog version, the upper range of the abs max for the SW pin is simply due to the body diode of the high side FET. Applying a voltage at SW greater than 0.3V above the voltage at the…
If DVDD3318_A, DVDD3318_B, or DVDD3318_C exceed STATIC 1.8V by more than 2V, can this damage the chip, or just cause a malfunction? This will not be a problem on power-up, but on power-down the decay of the supplies depends on how much power is…