Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQ27Z561 , BQSTUDIO , EV2400 Tool/software: Hi,
I have created a golden image for my battery using the BQ27Z561 EVM, and it works correctly with the EVM. However, when I tested it with my custom…
This is the desired behaviour for our application, as this would prevent the Remaining Capacity and RSOC to prematurely drop to 0% at the end of the discharge. So, we want to keep this setup for product 1. We want this behaviour on product 2 as well but…
Daniel,
As per the Data manual of C6655/C6657, the maximum data rate is 1333 MT/s
-----> page no:7 https://www.ti.com/lit/ds/symlink/tms320c6655.pdf
In your design, you selected " DDR3 (4Gb, 1600Mbps )".
Please note, while calculating…
Hello,
these are the information I got from the monitors on the RX gain and the PMCLKLO
RXGainPhaseMonitoring: RX gain: 15, 0, 0, 20, 20, 20, 281, 268, 270, 293, 290, 279, 280, 296, 295, 285, 283, 292, 3034, 3200, 3390, 2154, 8458, 8610, 8830, 7690, 21030…
Part Number: BQ34Z100-G1 Tool/software: Hi, I come back about this previous topic .
Here a log with BQ Studio : 8A - 7A - rest 30s.xlsx
Here the corresponding Data Flash : 8814.DF post LC amended.gg.csv
The "Number of series cell" is ok (7) ; the…
Part Number: TPS65994AE Tool/software: Hi,
We discovered a problem when testing "USB4 Systems Support DP Tunneling" (as shown below).
Port Reset fail
Fail Log as attachment
UCSI Get Connector Status command - USB device detection [Type-C MUTT…
Part Number: BQ34Z100 Tool/software: Hi
The battery pack is in good condition before shipment; After returning, it was found that FullChargeCapacity had been updated to 0mah, and RA had also been updated abnormally; The attachment contains the log and…
Hi, Daolin
Thanks your replies.
* Brief my test environment.
AM62EVB or customer's DUT connect to one of gateway port. I also setup another PC for iperf3 server, server also connect to one of gateway port.
gateway information as below :
https://www…
Part Number: AM62A7-Q1 We used the AM62Ax MCU+ SDK: Developer Guides (ti.com) to compile the emmc boot file and successfully started the AM62A. However, when I run the GST pipeline, the following error message appears:
APP: Init ... !!!
MEM: Init ... …