Other Parts Discussed in Thread: TPS65265 Hi, Team
A car infotainment customer Flyaudio is using TPS65265 in their project. The DCDC2 is output 3.3V for eMMC.
When system power up, the output current will change between 0 and 300mA rapidly. And it makes…
Other Parts Discussed in Thread: TPS43061 , TPS65265 , LMC555 , TPS43060 , TPS55330 Hi,
I need to sync clock between TPS65265 and TPS43061. What is the most suitable external clock to be used for sync freq at 500kHz?
Part Number: TPS65263-Q1 Other Parts Discussed in Thread: TPS65265 Hi team,
How much volts is it for the dropout voltage of TPS65263-Q1 and TPS65265? Do we have the test data like below curve?
Hi Henry,
If the requirement of output current is 0.9V/2~3A, 3.3V/3A, 1.5V/1.5A, TPS65266 can not exactly meet your requirement since it can support 3/2/2A. You can take a look at TPS65265 which can support 5/3/2A. The recommend operating junction temperature…
Hi,
Now we are thinking f using multiple output PMIC IC.
We would connect a DAC output to the feedback pin (through a resistor) in addition to the fixed resistor feedback. If the PMIC has I2C interface for setting the voltage value, that will be an added…
Part Number: TMS320C6678 Other Parts Discussed in Thread: TPS65261 , TPS65265 Hi,
In the TI TMS320C6678 EVM Board Rev. 3A (DSPM-8301E) power consumption table written that DVDD1 (VCC1V0) current is 5A, when I used the "C6678_Power_Consumption_Summary_Rev3_4…
Hi, Kay
TPS65270 can compete MP2223.
Besides,
For larger loading and 2 channels, there are TPS65273V, TPS65276V, TPS65279.
And there are 3 channels devices, TPS65261, TPS65263, TPS65265.