Part Number: TPS65982 Other Parts Discussed in Thread: TPS65987DDK , TPS65988DK , TPS65987D , USB-C-PD-DUO-EVM , TPS65987DDJ , TPS65987DJEVM Hi, TI expert
There is an inquiry from a customer about PD controller recommendation.
Application: Cradle The functions…
Hi Danilo,
Both EVMs are capable of 100W of transactions, however this will be dependent on the cable's capability (needs to be 100W capable). As you probably already reviewed, the DUO EVM is a two-part EVM that includes a Source and Sink board (both…
Part Number: TPS65987DDJ Other Parts Discussed in Thread: TPS65987DJEVM , TPS65987 , TPS65987D
Hi,
I'm evaluating TPS65987DDJ capabilities using TPS65987DJEVM evaluation board which is connected to an iPad has a builtin USB-C port.
I want the evaluation…
Hi Phillipe,
Sorry for the confusion, I should have checked this earlier. You currently have the TPS65987DJEVM (with the DJ pd controller) on hand. The TPS65987DEVM has the DH version of the PD controller. I have been testing the DH version on my end…
Hi Francois,
François Bernard said: -Will the PC work in display port alt mode even if it supports Thunderbolt ? I assume that if it supports Thunderbolt it will supports DP alt mode
The TPS65987EVM(Which has the TPS65987D) does not support TBT. None of…
Hello Emma,
So, to answer your question, we are using the TPS65987DJEVM .
On another note, we had to put on hold the testing on this project to finish an urgent one just for week or 2. I will give more details and results as soon as we resume the testing…
Hello Adam,
I am the customer having this issue. I have tried the versions of the FTDI drivers in the above link but no success.
I just want to confirm that if I purchase the Aardvark device, that I will not have this issue.
The TPS65987DJEVM evaluation…
Hello Kedar,
I am attaching the PD controller State Log as you requested. I don't have a PD analyzer to capture the CC line traces. This failure not only occurs with our design but also with the TI TPS65987DJEVM evaluation module. On the scope I…
Hello,
Please follow the programming steps outlined in the users guide to ensure you are programming the source board and not the sink board.
Also, if you press the 20V button, it will act as the TPS65987DJEVM board, with no need to re program the bo…
Hello,
I would not recommend using the TPS65987DJEVM as this is a different device that is geared towards host thunderbolt platforms.
You could use an Aardvark as that is a tried and true method for I2C interaction. You can also use the aardvark to flash…