Part Number: TPS65988DJEVM Other Parts Discussed in Thread: TPS65988DJ , , TPS65988DKEVM , TPS65988DK , TPS65987DDK Tool/software: Dear TI, I have set up the IC using the Application customization tool new project as TPS65988DH, Standard, dual role port(DRP…
Part Number: TPS65988DJEVM Tool/software: Dear TI support, I want to attach a USB C supply as source without having the EVM powered from the external jack then attach a sink device on the other USB port to charge it. I can make this work if I sort VBUS…
Hi Andrew,
I did confirm that in the source power role, the TPS65988 cannot force the contract negotiated to be the variable PDO. The far-end sink side PD will request either the fixed 5V PDO or the variable 5-9V PDO. Whichever PDO it requests is the…
Part Number: TPS65988DJEVM Other Parts Discussed in Thread: TPS65988DJ Hi, I have two questions.
1. The chip on my eval board has a a suffix of DJ and that option does not appear in the part selection menu of the configuration tool Only DH and DK.
2.…
I found that there was a problem with the soldering of the TPS65988. LDO_3v3 was not connected. Now I am able to read and re-program the flash on the EVK
Part Number: TPS65988DJEVM Most of the Ti reference designs use PPHV1/2 for the fixed SYSTEM_5V rail for Sourcing power, and the external powerpaths (controlled by PP_EXT1/2) for PD sink to the BQ charger.
Instead, can I use PPHV1/2 for PD Source & Sink…
Part Number: TPS65988DJEVM Other Parts Discussed in Thread: TPS65988 Hi,
I need to configure the TPS65988 EVM in sink configuration. To perform the configuration loading i am using FTDI but getting below error message. pl let us know how to resolve the…
Hi Matt,
Thanks for your reply. Since we have already bought a TPS65988DJEVM in the market for testing, may we know what are the difference between TPS65988DJ and TPS65988DK? Could we still create a project by choosing TPS65988DH/ TPS65988DK in the Application…
Part Number: TPS65988DJEVM Hello,
On the TPS65988EVM user guide schematic, Q16/Q18 looks to be a P channel MOSFET. However, on the BOM located in the TPS65988EVM user guide, Q16/Q18 is shown to be NX3008NBKW,115 which is a N-CH MOSFET. Typically, I would…
Part Number: TPS65988DJEVM Other Parts Discussed in Thread: TPS65988 , Tool/software: Hi Team,
I have a TPS65988DJEVM to evaluate the PD controller TPS65988. The Debug Interface on the Evalboard is TIVA. I could connect and configure the board using Application…