Part Number: TPS66120 Hi Team
do we have any proper replacement for KST1697A>
https://www.kinet-ic.com/uploads/KTS1697A-04a.pdf
I have checked the cross reference.
TPS66120 EN pin is active high so it can't match customer applicaiton.
B…
Part Number: TPS66120 Other Parts Discussed in Thread: TPS25948 Hi team, my customer need a USB type C PD power switch and the current limit is about 7A. However, I only see TPS66120 on the website, which current limit is 5A. Are there any other products…
Part Number: TPS66120 Other Parts Discussed in Thread: TPS66121
Hello,
In the datasheet Vt+ and Vt- mentioned as percentage. Is it the enable VIH and VIL parameter?
Note: Our PD controller enable out pin is 1.8v by default.
Part Number: TPS66120 In the page 17 from the datasheet SLVSEW9B –AUGUST 2019 –REVISED DECEMBER 2019 there are some descriptions of the conditions to change of status. The first 2 conditions seem to change from the pin EN1. I cannot find EN1 pin…
Part Number: TPS66120 Other Parts Discussed in Thread: TPS66020 Hello expert,
Customer is wondering if we can use TPS66120 on source out side to support 5V~20V. Since I saw this solution is designed for sink power path and need to use with 5V power path…
Part Number: TPS66120
Dear Team,
From the spec, TPS66120 should be able to supply LDO 3.3V/ 30mA(maximum) to peripheral device.
But a lot of device like MCU requires more than 30mA current capabilities.
So my customer would like to know in the application…
Will,
It looks like you're running into an issue with the discrete power path implementation on the TPS65988EVM. It will likely be easier to use two of the TPS66120 power path ICs instead of this discrete circuit. The TPS66120 integrates reverse current…