Part Number: TPS22995H-Q1 Other Parts Discussed in Thread: TPS74801-Q1 , , LP8764-Q1 We are using one SSD part for that we required 3 power rails 3.3V, 1.2V & 0.9V .We are using TPS22995H-Q1 for power supply 3.3V , TPS74801-Q1 for 1.2V supply & LP8764…
Part Number: TPS74801-Q1 Other Parts Discussed in Thread: TPS74801 Hi Sir,
My customer looking for LDO with below condition,
Input: 2.5V~5V
Output: 0.9V/1.5A
Q-Grade
I suggest using TPS74801-Q1 for them, pls help for questions from customer as below, …
Hi Gunter,
If you intend to have a safety system, LDO recommended for 1.2 V is TPS7A88-Q1 which will meet the power requirements. For non-safety application, LDO recommended for 1.2 V is TPS74801-Q1.
Thanks,
Susmitha.
Part Number: TPS74801-Q1 Other Parts Discussed in Thread: TPS7A54-Q1 Hi,
We are planning to use the TPS74801-Q1 or TPS7A54-Q1 for our application. Need suggestion which part is best for our need and support from TI:
1. Vout= 1.24V, Iout= 0.3A , Vin= 1…
Part Number: TPS74801-Q1 I'm using this part in the configuration:
Vin = 5V
Vout = 3.3V
The datasheet specifies that Vbias be at least 1.6V higher than Vout. My configuration satisfies that requirement (with 0.1V to spare) and so I plan to connect…
Part Number: TPS74801-Q1 Hello team,
Could you please advise with the design team what the purpose of C22 (loop capacitor) in the schema below (CODE IDENTITY NUMBER 01295)?
according to the LDO eval board, this capacitor is not implemented.
Thanks in…
Tejas:
Q1:VDD33/VDD11 is supply name for hub device, BOARD5v and board_3p3v or board_1p1v are supply name generated from LDO on the board. VDD33/VDD11 are only for hub device, BOARD_xV are for all other devices on the board, like LDO, EEPROM. so you do…
Part Number: TPS748A-Q1 Other Parts Discussed in Thread: TPS748A , , TPS74801
Hello,
Normally,LDO output Vout = Vfb*(R1+R2)/R2,there is no description in the datasheet, dose tps748a Vout be set by Vfb, R1, R2?
And, is there any output fixed version, i…
Part Number: IWR6843 Other Parts Discussed in Thread: TPS74801-Q1 Hi there,
I might have came accross a few inaccuracies regarding the IWR6843 documentation:
- In HardwareDesignChecklist_V0p8_IWR6843.xlsx / Customer IO List I am missing ball B11 VIN_18CLK…