Part Number: TPS79501-Q1 Hi Sir,
I didn't see the AEC-Q100 qualified wording in the datasheet..
I only saw the automotive application.
Can you confirm it if it passed Q100?
thanks.
Alpha
Part Number: TPS79501-Q1 Other Parts Discussed in Thread: TPS735 , TPS795 Hi Sir,
My customer is looking for a P2P second source to replace LD39050PU33R, I could not find a exactly P2P device on ti.com.
Could you kindly help?
The package of LD39050PU33R…
Hello Jiawei,
Here is an application note for how to design an external soft start circuit: /cfs-file/__key/communityserver-discussions-components-files/138/1616.Soft_2D00_Start-Circuits-for-LDO-Linear-Regulators_5F00_slyt096_5B00_1_5D00_.pdf
Also…
Hey Chen,
Is the EN signal distorted before VOUT goes high because of a probe connection issue?
Is the output load a resistive or electronic load?
I think the internal soft start of this part is limiting the output of the device.
This white paper…
Zeev,
The TPS73801-SEP does not have a soft start circuit.
Currently the only space grade LDO with integrated soft start is the TPS7H1101A-SP .
There is a TI application note on adding soft start to an LDO externally. This may or may not be a suitable…
Part Number: DCR011205 Other Parts Discussed in Thread: DCR011203 I am using several DCR01 regulators in one of my designs. There are two sets of 3, one DCR011203 and two DCR011205s. Both sets have completely independent loads. They have sync pins tied…
Hello Tapajit,
Commonly the SN6501 receives its input voltage, Vin, from a regulated output of a linear regulator (LDO). The soft-start is therefore applied to the output voltage of this LDO. As there are various options on how to design a soft-start…
Hi Jonathan,
I'm trying to get these pushed to TI.com but I have attached them here for your use.
Regards, Bill
Daughtercard BOM
am335x_gpevm_gpdboard_3H0001_bom_rev1_2b.xlsx
LCD card BOM
am335x_gpevm_lcdaboard_3H0005_bom_rev1_3a.xlsx
Hi Board Designers,
Inputs related to PDN - Inputs related to DDR3 interface capacitors recommendations for processor and memory device
https://www.ti.com/lit/ds/symlink/am3358.pdf
7.7.2.3 DDR3 and DDR3L Routing Guidelines including capacitors …