Part Number: LM5069QUICK-CALC Other Parts Discussed in Thread: LM5069 Hi,
We are using LM5069-2 IC for hot swap application, below are the specs:
- Vin = 24V +/-10% tolerance
- Current Limit : 10A,
- Max load Capacitance : 2200uF
- Ta : 60C
- Power limit…
Dear Orlando,
Out max output current is 14.5A, which is lower than 16A. We will use heatsink for heat dissipation. The Irate of inductor we chosen is 24A, which can meet the requirement.
Your reply is very helpful. Thank you very much!
Part Number: AM62X-PET-CALC Hi TI
For UG1V8_VDDA power rail , current current consumption result is Max current = 100mA, can you help assess whether this is make sense?
If the current is make sense , please help review this power rail layout design …
Part Number: FLYBUCK-FLYBACK-DESIGN-CALC Other Parts Discussed in Thread: LM5155 , LM5156 Hello, We are wondering if there is any suitable controller and circuit or calculator for the design of a flyback topology DC/DC converter that can meet the requirements…
Part Number: LM3423-Q1 Hi Team,
since Webench does not support LM3423-Q1 design anymore, can you please share your design guides and/or calculator sheets for LM3423-Q1 designs? I could not find any of them online in the product folder. It would be quite…
Part Number: UCC25600-DESIGN-CALC Other Parts Discussed in Thread: UCC25600 Hi
We are designing LLC resonant converter using UCC25600. if there is already existing mathcad file please share with us.
Regards
Nitesh Kr Jha
Part Number: LM5141DESIGN-CALC Other Parts Discussed in Thread: LM5141 The design tools I believe maybe incorrect. According to the latest rev.D datasheet page 16 equation 4 is states:
However in the Design Tool provided Rfb1 and Rfb2 are swapped. Shown…
Part Number: LM5145DESIGN-CALC
I want to design in the case of negative output using LM5145DESIGN-CALC.
However, It seems that it can only be designed in the case of positive output .
What should I do?
I want to observe the figure of Bode-Prot, in the…