Part Number: TRS3221E Hello, I am currently using the TRS3221EIPWR with autoshutdown disabled and 4.9V power rail to VCC. The circuit operates as expected and meets all the voltage thresholds with the uController. I am simply curious why the ROUT VOH…
Part Number: TRS3221E Hi, Good day. Our customer is using the TRS3221E and they have an inquiry about their application. Kindly see the details below. "I have an application where the D-out of the RS232 transceiver TRS3221EIRGTR is also connected to a…
Part Number: TRS3221E Hello,
I have a question for TRS3221E. The datasheet specifies I_CC(supply current) with only No Load condition as 1mA Max My customer would like to confirm the power consumption at 9600bps. Do you have any data that shows power consumption…
Part Number: TRS3221E Hi,
I would like to ask you about the TRS3221EIDBR specification,
TRS3221EIDBR’s TYP Maximum Data rate=250kbit/s @ Ta=25°C,
What is the maximum data rate under the conditions of Ta=0°C and Ta=40°C? Thank you.
…
Part Number: TRS3221E Hi,
I need to know what the switching frequency is for the internal charge pump on the TRS3221E. I need to perform harsh military EMI/EMC qualifications and want to catalog all the fundamental frequencies that are present on the…
Part Number: TRS3221E Hello TI interface team!
I have to make up a interface adaptor containing, among other parts, a RS232 <-> RS422 conversion.
For those I have selected the abovementioned components. They are directly coupled back-to-back by…
Part Number: TRS3221E Other Parts Discussed in Thread: SN65HVD21 Hello,
Is there a solution to use the same two wires for combining both 232 and 485 communication?
Thank you
Part Number: TRSF3221E Other Parts Discussed in Thread: TRS3221E Hi,
Please help to recommend a product for battery power supply, hoping that the static power consumption is small, the speed requirement is very low, and the package is also small.
Thank…