Part Number: TRSF3221E Other Parts Discussed in Thread: TRS3227E
Tool/software:
Hi Team,
1) What's the difference between TRSF3221E and TRS3227E?.
2) What's the difference between Auto-powerdown(TRSF3221E supports) and Auto-powerdown plus(TRS3227E…
Part Number: DS90LV047A Other Parts Discussed in Thread: TRSF3232 , TRS3227E , I am using the parts mentioned above to provide LVDS signaling over a long length of Cat5E cable (4 signals total). The LVDS segment seems to work well. Two of the signals…
Other Parts Discussed in Thread: TRS3122E , TRS3227 , TRS3227E , MAX3227E , MAX3227
Number of Drivers/Receivers
1/1
Duplex
full
Supply Voltage
1.65V to 5.5V or 1.8V to 5.5V
Data rate
250Kbps and 1Mbps
Channel
single…
Part Number: TRS3122E Other Parts Discussed in Thread: TXB0104 , TXU0204 , TRSF3223E , TXU0304 , TRS3227E , MAX3227E ,
Our requirement is to have a 232 transceiver with a 1.2V logic level of FPGA bank operating at 921.6 Kbps. As we could not find any…
Gilad,
Thank you for your question.
Please consider the TRS3227E RS-232 tranceiver (1Mbps, 3.3V-5V supply range, single channel, with Enable). The datasheet may be found here:
TRS3227E DS
For your UART inquiry, do you have a preference for number…
Hello, Ron Michallick:
Did you means:
If I use powerdown function, when TRS3227E in powerdown mode, I must first send a unuse data, then wait a while or read the READY pin, then I can send my own data? And this unuse data may cause recive a unknow…
Dustin,
The TUSB1105 is a USB transceiver or PHYsical layer. It is purely the analog electrical signalling portion of a USB device. It can only be used in conjunction with MCUs/application processors that have the digital USB core integrated on chip…