Part Number: TRS3243E Hi there,
I am using this device to translate RS232 signal levels to control status LEDs, however I am not using all the RIN and DIN. My question is: Is there a standard configuration for unused pins - open, tie to GND or tie to…
Part Number: TRS3243E The theta_JA and maximum ambient temperature limit are provided in the data sheet. What are the max junction temperature limit and the theta_JC values for this part (TRS3243EIPWR)?
Part Number: MAX3243 Other Parts Discussed in Thread: TRS3243 , , TRS3243E , Hi Sir,
What are the differences among MAX3243, MAX3243E, TRS3243 and TRS3243E? Thanks!
Best regards,
Sam Ting
Part Number: TRS3243E Other Parts Discussed in Thread: TRS3243 Let me confirm just in case whether the power-pad in TRS3243 should be connected to GND.
Thanks and Regards,
Metropolitan (Tokyo) Area FAE Kenji Ninagawa
Part Number: TRS3243E Hi Team,
My customer use TRS3243E to connect a Cash Drawer device. The Cash Drawer side shorted pin1(DCD)/pin4(DTR)/pin6(DSR), so it would cause they are all 12V.
We found if 12V input to DOUT, the V+ voltage would be abnormal, and…
Part Number: GD75232 Other Parts Discussed in Thread: GD65232 , SN75C185 , TIDA-00557 , TRS3243E Hi Team,
I would like to apply for the EVM of GD75232 for customer, but I cannot find it in ti.com.
Is there the Evaluation Module designed for GD75232? If so,…
Other Parts Discussed in Thread: TRS3243E , DS3486 Hi Sirs,
As title, we have use TRS3243E.
We need confirm does TRS3243E support EIA423 signal??
Have any risk??
Thanks for your help.
Other Parts Discussed in Thread: TRS3243E Hi Sirs,
Sorry to bother you.
We would need confirm that what is TRS3243E data rate when use in the 15m cable?? We saw min is 250k/ Typ is 500k.
So should be between this, right??