Part Number: TS3USB30
Currently I am building a circuit to control using an Arduino the flow communication between Android-PC and Android-Microcontroller, since the connection android-PC requires android to be in accessory mode, and the connection Android…
Part Number: TS3USB30 Hi team
In the customer's last-gen project, the USB flash drive could be detected successfully. The signal chain is as follow:
USB interface -> TS3USB30 -> ADUM3160 -> Processor
However, the customer found that this…
Part Number: TS3USB30 Hi Dear experts.
My customer wants to use TS3USB30 to support below MUX function for LVDS signal for differential or single ended signal, the max LVDS frequency is 100MHz.
Can TS3USB30 support? From the block diagram, should be ok…
Part Number: TS3USB30E Other Parts Discussed in Thread: TS3USB30 Hi Team,
What's the internal connection between D1+/D1-/D2+/D2- and Vcc?
The test shows that there is power-off protection( https://e2e.ti.com/support/switches-multiplexers/f/388/t/65…
Part Number: TS3USB30E Hi Team,
When Vcc is 3.3V, the IO impedance is very low, while the IO impedance is very high when Vcc is 0V.
May I know when IO becomes high impedance if Vcc starts to drop from 3.3V?
Thanks and Best Regards!
Hao
Part Number: TS3USB221 Other Parts Discussed in Thread: TS3USB30E , TS3USB3000 , , , I want to implement a USB2.0 multiplexer (mux) into my system, and have certain requirements for the functionality of the mux. What choice would be best for my system?
Part Number: TS3USB30 Hi team,
As title. TS3USB30 damage when VCC and OE# without power ?
Customer want to know if there any risk when Vcc=0V and OE# =0V but D+D- have signal.
Thanks
Shaq.
Part Number: TS3USB30E Other Parts Discussed in Thread: TS3USB221 Hi,
we have usb switch for USB2.0 like TS3USB30E.
Now my customer need to upgrade the port to USB type C, but it's not a real typeC, they only add CC1 for PD handshaking, ID for OTG setting…
Part Number: TS3USB30 K-Free Technology Limited uses the SPDT switch of TI: TS3USB30ERSWR, And there are about 6% of the functional failure problems in the PCBA downloading software and the RF calibration station. The hardware design schematic is such as…
Part Number: TS3USB30E Hi Sirs,
Sorry to bother you.
For DEMUX SW TS3USB30ERSWR if it no connect the VCC power, what is the switch D+/D- behavior ? It still can work ?
Our application as indicated below, DEMUX SW connect to USB2.0 signal, but +3P3_DEBUG…