Part Number: TS3USB30 e2e,
I would like to know whether it can be powered from VBUS at 5V. the datasheet spec for Vcc runs upto 4.3V so I’m inclined to say that is not supported. The max rating does go up to 7V but I think that’s not for extended periods…
Part Number: TS3USB30 Hi team,
My customer use the TS3USB30 in server to transmit the PCIE 100M clock and show the abnormal propagation delay and the output voltage.
Below is the schematic
Below is signal capture of the SEL and the input signal and…
Part Number: TS3USB30E Hi,
Could you please check the current consumption with VCC=3.3V, OE=3.3V and S=3.3V?
The datasheet explains that <0.1uA when VCC=4.3V, I_I/O = 0, Switch ON/OFF. Can I think about condition takes <1uA?
Regards, Nagata.
Part Number: TS3USB30 Hello Team ,
my customer wants to interface 2 USB device ( WIFI dongle and a USB storage stick ) simultaneously . his uC has single USB port .
We are confused if we have to go for a USB hub or a USB mux will do the job .
Can you…
Part Number: TS3USB30 Hi,
Do we have an EVM for TS3USB30? My customer would like to evaluate this device and I did not see it in the product folder.
Thanks,
Chuchen
Part Number: TS3USB30 Hello,
I am looking for the IBIS model for TS3USB30 IC.
Could it be provided as it is not available in TI website.
Thanks and regards,
Nishmitha
Part Number: TS3USB30E Hi,
Can you provide me the differential pair routing guidelines for the VSSOP package of TS3USB30E IC?
While routing the IC, I am having some issues because of PIN configurations.
Thanks and Regards,
Syed Imthiaz.