Ranita,
To determine if a signal switch can support a specific signal standard such as HSiC you need to evaluate the signal standard's voltage/current levels and the datarate/bandwidth.
When I googled the HSiC signal standard I find that it is a two…
Other Parts Discussed in Thread: TS3USB3031 , TS3USBA225 Hi all Would you mind if we ask TS3USB3031? We are looking for USB2.0 switch which is 1:3 SP3T (1:3 MUX/DEMUX). So, we recognize that TS3USBA225 is avliable to use USB2.0 switch as 1:3 SP3T.
About TS3USB3031…
Other Parts Discussed in Thread: TS3USB3031 Customer uses TS3USB3031 on a project but finds lots of failure on Pin 6, which will show a low resistance on their board(less than 100ohm), but if they pull high this pin to 3.3V, the resistance will become…
Other Parts Discussed in Thread: TS3USB3031 We need a very small footprint chip and a very low propagation delay to select between different clocks in our boards. A clock switch has too much propagation delay or part to part skew. We are using this switch…
Other Parts Discussed in Thread: TS3USB3031 , TS3USB3000
question on behalf of customer:
Do we have a dual SPDT switch like two MHL/MyDP channels of the TS3USB3031? It sounds like they like our TS3USB3031 but don’t necessarily need the extra channel…
Other Parts Discussed in Thread: TS3USB221 , TS3USB3031 Hi Sir,
Our customer survey the USB 1:3 and 1:2 switch, we are promotion the TS3USB221 to 1:2 case used.
But see the TS3USB3031 datasheet is similar function, Does the TS3USB3031 can be use on USB…
Other Parts Discussed in Thread: TS3USB3031 , TS3USB3000 Hi Team,
I have a few question on the TS3USB3031I was hoping you could answer:
1. If the device is powered from 2.7V, this has no effect on the maximum signal voltage that can be passed through correct…
Other Parts Discussed in Thread: TS3USB3031 Hi,
I'd like to ask about TS3USB3031.
Is it possible to swap +/- signals?
(to connect minus signals of differencial to D+/MHL+/USB1+/USB2+ and plus signals of differencial to D-/MHL-/USB1-/USB2-)
I think it…
Part Number: TS3USBCA4 Other Parts Discussed in Thread: TS3USB3031 Dear TI experts,
I'm considering the TS3USBCA410 as a replacement of the currently unavailable TS3USB3031 in a non-demanding application (UART up to 1Mbps).
Unlike other devices, there…
Other Parts Discussed in Thread: TS3USB3031 Hi team,
I can understand TS3USB3031 is MyDP and dual USB 2.0 High-Speed switch.
Is it possible to use the device as MyDP 1:3 switch?
My customer want to use this device as MyDP 1:3 switch.
Best Regards,
Yaita…