Part Number: TS3USB31E Hi Team,
Customer is designing usb application.
There is no EVM for TS3USB31E (8-pin UQFN, RSE package). Is there any multi-function TI EVM can mount this device for evaluation?
BR,
SHH
Part Number: TS3USB31 Other Parts Discussed in Thread: TS5USBC402 Hello Team
When TS3USB31 vdd is 5V, Can apply 5V to D+/D- line? what will happen when applied?
If not, could you suggest a solution to replace AZAW2110S?
Part Number: TS3USB31E Other Parts Discussed in Thread: TS5USBC41 , TS5USBA224 Hi Sir,
We are looking for a DPST(Double Pole, Single Throw) switch, which working at 5V,
And found TS3USB31E is suitable for the function but the VCC is 2.25 V to 4.3 V only…
Part Number: TS3USB31E Hi team,
If customer wants to save GPIO pin to control OE pin of TS3USB31E, can they directly tie it to ground? In this case, the device will still shut down the switch when Vcc<2.25V and directly open when Vcc>2.25A?
Thanks…
Part Number: TS3USB31
Hi Sirs,
Sorry to bother you.
Generally,the incoming and outgoing lines should be parallel? How is 2 in 3 out, 5 in 6 out
Is this going to be smooth?
Look at the block diagram & Package, HSD1+ is connected with D+, HSD1- is connected…
TI has a large variety of 2-channel USB2.0 passive muxes, most coming with a feature or functionality that appeals to a certain use case. Depending on what your use case is, there is likely a USB2.0 mux that supports it.
For starters, if you are looking…
Part Number: TS3USB31E Other Parts Discussed in Thread: TS3USB31 Hi,
My customer wants the IBIS model for TS3USB31ERSER.
Can you help to check if we can provide this model?
Thanks a lot.
Oliver Ou
Part Number: TS3USB3000 Other Parts Discussed in Thread: TS3USB31E , Hi all Would you mind if we ask TS3USB3000 and TS3USB31E? There is description each datasheets as follows; <ABS Maximum ratings VI Digital input voltage (SEL, OE)> TS3USB3000 : 5.5V TS3USB31E…
Part Number: TS3USB31 Since the specifications of all the ports are the same and the switches are passive:
It it possible to connect the USB_D + signal to the TS3USB31_D - ? And vice versa?
Part Number: TS3USB31E Hi,
The recommended operation voltage range for Vcc is from 2.25V to 4.3V. Considering we're using it for D+/D- @ 3.3V, should we always choose 3.3V to be the Vcc level? Any other consideratin here?
Thanks!
Antony