Part Number: AM625 Other Parts Discussed in Thread: TSC2046 , ADS7846 Tool/software: Hi Expert,
Linux version: 5.10.184-cip36-yocto-standard
When a customer uses tsc2046, it needs to be pressed very hard to get a response.
Is there anything that…
Part Number: TSC2046 Tool/software: hi sir
I use TSC2046 as a touch screen sensor
I need to press the button hard and the TSC2046 accepts it. If I touch the button lightly, the TSC2046 does not receive the signal.
How to improve touch sensitivity…
Part Number: TSC2046 Hi team,
After customer set the device mode, there are some interrupt signal(the top most). Is this a normal situation?
Or how to solve the problem?
Part Number: TSC2046 Hi team,
I have a question about the interface between the host and TSC2046EVM-PDK USB.
Can it work with the HID standard drivers included in the Linux kernel?
Best Regards,
Part Number: AM625 Other Parts Discussed in Thread: TSC2046 , , SK-AM62B , SK-LCD1 In our custom AM625 SOM we've used touch IC TSC2046 and now I want to configure it using the device tree structure files, so that I can use touch feature for AM625 SOM…
Part Number: TSC2046 What is the battery drain current flow into VBAT pin in case of unpowered TSC2046 IC?
I think to situation, when VBAT pin is connected to battery, but there is a power switch between battery and DC/DC converter and is switched off…
Part Number: TSC2046E Other Parts Discussed in Thread: TSC2046 Hello guys,
One of my customers is looking for a touch panel controller and they considering using TSC2046E.
At this moment, they have the following questions. Q1. Is the deference point…
Part Number: TSC2046 Other Parts Discussed in Thread: TSC2008 , 1) Development board: We need the development for the testing purpose so kindly send us this if available.
2) Supply current (operating current and standby current)
3) ESD (electrostatic…
Part Number: TSC2046 Dear Specialists,
My customer is evaluating TSC2046 and have questions.
I was grateful if you could advise.
---
Regarding TSC2046, The sequence below is not followed. What could be the cause?
・At the start of DOUT, BUSY…
Part Number: TSC2046 Hello,
We have noticed that some of our products using the TSC2046 have an unresponsive touchscreen. This seems to be because the detected coordinates are changing and not stabilized. I have noticed that on the PCBs that exhibit…