Part Number: TUSB1146 Hi
May I ask a question, what is the bandwidth of dp alt mode under only dp0/1? According to the specification, dp0/1/2/3 is 10gbps, right?
Part Number: TUSB1146
Hi team,
what's the definition of this 8.5dB at host device?
for example,
if the total PCB loss is 20dB, and our redriver can compensate 12dB, which means we still have 8dB loss left which is within the USB host spec (8dB<8…
Hi David,
thanks a lot
BTW, I correct my last question to " -1dB emphasis can exactly compensate 1dB PCB loss ideally"
in case you miss my question meaning.
Part Number: TUSB1146 Hi,
Would you please help to review TUSB1146 schematic?
Please add me friend, I will send schematic via privacy message.
Thanks!
Jeff
Part Number: TUSB1146 Hi team,
two question from my customer,
1. would you send the loss budget of the VESA DP1.4/2.1 materiel to me offline?
2. they want to know if there's a insertion loss inside the MUX of the TUSB1146, or any insertion loss after…
Part Number: TUSB1146 Other Parts Discussed in Thread: TPS65987D , Hello,
I'm working on a DFP design using TUSB1146 and TPS65987D and would like to try using AEQ since I'm unsure of the final channel length which will probably be a mix of cables or…
Part Number: TUSB1146 Hi,
when i want to use the the TUSB1146 in USB 3.1 +2 Lane DP, can left the remaining DP inputs or should they be connect to any voltgage.
Can I provide the schematic for a review to TI?
thanks
Michael
Part Number: TUSB1064 Other Parts Discussed in Thread: TPS65987D , TUSB1146 , I have two ports in my design, both ends have the TPS65987D to control the Display Port 3.0 Mux.
TUSB1064 on the UFP side and TUSB1146 on the DFP. A USB hub in between and the…
Part Number: TUSB1146 Hi Team,
as noted in the datasheet of TUSB1146, the device supports USB Type-C Alt Mode interfaces such as HDMI Alt Mode. My customer was able to setup the host side like it is described in the Application note:
www.ti.com/.../slla333…
Part Number: TUSB1146 Other Parts Discussed in Thread: TUSB1044 , TUSB544 Hi Team,
As title, Can TUSB1146 support USB3.2 gen1 x2 (10G)? If yes, does we have reference schematic can provide to customer ?
If not, does we have any other redriver or retimer…