Part Number: TUSB1210-Q1 Tool/software: May I connect 5V for VBAT voltage?
Figure 5 Host or OTG, ULPI Input Clock Mode Application Diagram
Figure 5 shows a diagram for connecting 3.1V-5.5V.
Part Number: TUSB1210-Q1 Hi all,
I would like to know some questions about TUSB1210-Q1.
When using under the following conditions, the DP/DM is reversed.
This does not change even if register 0x08 is rewritten.
<conditions>
High-speed
Vbus=3.3V …
Part Number: TUSB1210 HI,Team
I am considering whether to adopt TUSB1210 or TUSB1210-Q1. Please tell me the following about TUSB1210 and TUSB1210-Q1.
【question 1】 ・I checked the contents of the datasheets for the TUSB1210 and TUSB1210-Q1, but I couldn't…
Part Number: TUSB1210-Q1 Other Parts Discussed in Thread: TUSB1210 hi Team
Customer uses TUSB1210 to hang out of the FPGA with ULPI interface inside the FPGA to interface with TUSB1210, TUSB1210 to connect to the PC, would you like to ask if additional…
Part Number: TUSB1210-Q1 Team,
Could you confirm us, if the TUSB1210BRHBTQ1 and TUSB1210BRHBR are the same die?
What additional tests are performed for the Q1 qualification?
Thanks in advance.
- Needhu
Part Number: TUSB1210-Q1
Hi team,
I got a question from customer.
"
I generated a very simple project by CubeMX, wanting to test the speed of the new usb2.0 phy. I've changed nothing. However, the VDD18 power supply would turned to about 2.8V after…
Part Number: TUSB1210-Q1 Other Parts Discussed in Thread: TUSB1210 Hi team,
TUSB1210-Q1 has 1.8V I/O level while my MCU is 3.3V I/O.
I don't want to use level shifter to minimize space of the board.
Could you advise alternative device which has ULPI…
Part Number: TUSB1210 Hi TI team,
We need your help to check our customer concerns regarding the communication Issue using TUSB1210-Q1 and Zynq 7045.
They are using a TUSB1210-Q1 USB Phy on a backplane card that allows a Zynq 7045 to communicate to an…
Part Number: TUSB1210-Q1 Other Parts Discussed in Thread: TUSB1210 Hi,
What is the reason why usb PHY doesn't work in high speed mode under Linux system? Is it because the driver software under Linux system needs to be updated?
The main processing…
Part Number: TUSB1210-Q1 Hi,
In my design , the TUSB1210-Q1 is in output clock configuration mode,so how long can I deassert reset signal after VDDIO/VDD18 is ok? just as the following picture described.
Thank you.
Best Regards.
Gavin