Hello,
Good to see that the device is working. Is this done with the settings as listed in your previous post, BOOST level 3 and RX_SENS level high?
The TUSB216I does have I2C registers which, if you want to use them, can go past the levels of boost and…
Part Number: TUSB212 Hi Team,
Could you help to check the schematic? There seems to be a issue with the connection of pin2/1 and pin 7/8, please help to check.
The same label is used in the schematic of the TUSB212 EVM, which may confuse customers.
…
Part Number: TUSB212
This is customer waveform.their config is DC=80mV, AC=3 , ENA_HS with a 27K pull-up and EQ is float.
The buffer/redriver is near to the USB host, and test the sign in the host side. Then some sign is reduction like the waveform.
Why…
Part Number: TUSB212 Hi expert,
My customer also have similar problem as the post
TUSB212: USB Host mode is not recognized
Sometimes can detect USB but sometimes can't. Is there any power up/down sequence need to be noticed? Or any other advise?
…
Part Number: TUSB212 Other Parts Discussed in Thread: TUSB216 , TUSB216-Q1 How much the maximum gain of the USB2.0 signal of TUSB 212? We want to make a USB2.0 10m extension cable, and plan to use one before and after the input and output respectively to…
Part Number: TUSB212 Hi team,
The host and salve would communicate with each other to identify what kind of usb device is before starting the data transmission with USB2.0. So during this communication, does tusb212 would regular the signal? I find…
Part Number: TUSB212 Dear Team,
I found that I adjusted the resistance of pin9, but the USB signal did not change. The following is the circuit connection, please review and analyze the reason? What else can be adjusted to change the waveform.
eye…
Part Number: TUSB212 Hi
My customer want to know if they want to bake the TUSV212 before SMT to avoid steam, what’s the baking temp and time for redriver?