Part Number: TUSB211-Q1 Other Parts Discussed in Thread: TUSB214-Q1 , TUSB214 , TUSB211 , TUSB217-Q1 , TUSB216 Hello team,
My customers ask some qustions if TUSB211-Q1 + TUSB214-Q1 can be used in their usb port for automotive application as diagram below…
Part Number: TUSB214-Q1 Other Parts Discussed in Thread: TUSB214 Dear TI sir
I use TUSB214-Q1 in a DA project to redrive the USB, but if I use old USB cable to connect Mobile phone or U-Disk to host, some time I find the USB device can not be find(happen…
Part Number: TUSB214-Q1 Do you mean that I must be reset device after changing I2C? Is it controlling RTSN? Please tell me how to reset and I2C setting sequence.
Hi Brian,
This issue on TUSB214-Q1 is not resolved yet on my customer's system board. Please help to reply to Charles Joen’s questions on TUSB214-Q1 asap.
Best regards, DY
Part Number: TUSB214-Q1
Hi team
I set AC boost and DC boost using I2C to TUSB214-Q1.
Sometimes, TUSB214-Q1 stop the function of AC boost and DC boost when it transmit packet while eye pattern measurement mode to CPU.
So, I set function by hardware but…
Part Number: TUSB214-Q1 Hi team.
I have heard that there is a way to set DC-Boost to 0mV using i2c.
I could not find anything about the 0mV setting in the datasheet.
Unable to find relevant data on the web too.
Please tell me how to set DC-Boost to 0mV…
Part Number: TUSB214-Q1 Hi team.
My customers do not want to use the DC Boost function of TUSB214-Q1.
MCU is not used, so it can not be controlled by I2C.
Can I control DC Boost with H/W only?
Or can you recommend Redriver with CDP function available…
Hi Koki-san,
1. TJ should not be 125C for either commercial or industrial variations. TJ limit for commercial part numbers is 85C and 105C for industrial part numbers. Are you referring to TUSB214-Q1 and TUSB217A-Q1?
2. There is not difference in the package…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TPS2549 , TUSB215 , TUSB214 Hi Sir
I saw TPS2549 have divider 3 and 1.2V detection
May I know TUSB215 can support apple 2.4A charge detection and samsung charge detection ?
Thanks