Part Number: TUSB215-Q1 Hello:
At present, My customer finds that Lotus has a demand for a front row Dual Port USB, which has two main functions:
(1) a USB port can support 60W fast charging; (2) Another port can support 27W fast charging and usb3 0 communication…
Part Number: TUSB215 Other Parts Discussed in Thread: TUSB216 , , TUSB217A , TUSB216I , TUSB212 Hello Sir:
We used TUSB216 for testing eye diagram, and already passed the Car play/ Android Auto testing.
But we are facing shortage issue, only TUSB215 has…
Hi Malik,
Thanks for your feedback. Customer will provide eye diagram for TUSB215-Q1 later.
As you talked before, TUSB216 is a better choice to replace TUSB217. Customer also want to evaluate TUSB216. There are two question need you help:
1. For TUSB216…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , , TUSB217 , TUSB215 Hi, We used to use tusb217-q1, but for some reasons, we now replace it with tusb215-q1. However, the following problems occur when using tusb215-q1. Please analyze what…
Part Number: TUSB215-Q1 Hi all.
Hope you can help with an issue.
Designed a circuit following the design example. MID boost while using a thin 1m cable that runs near motors.
When the board was connected to PC (no slave device) it shows up as failed to…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , TUSB213-Q1 Hi, For some reasons, we design the circuit of tusb215-q1 as shown in the figure below, that is, the 9th and 10th pins of tusb215-q1 are not connected, and the 5th and 6th pins…
Part Number: TUSB215 Other Parts Discussed in Thread: TUSB212 Hello guys,
One of my customers is considering using TUSB215 for their new products.
At this moment, they have the following questions. Could you please give me your reply for them?
Q1. Do you…
Part Number: TUSB215 Other Parts Discussed in Thread: TUSB217 , TPS2544 , TUSB213 Hi,
My customer is using TPS2544 and TUSB217, they are looking to qualify TUSB213 and TUSB215 as alternatives.
The TUSB is placed after the TPS2544 and the TPS2544 has a CDP…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TPS2549 I have both TPS2549 and TUSB215-Q1 in our design and I am wondering how USB role switching can be handled?
Do I need to configure TUSB215-Q1 via I2C when our system is in device mode?
regards…