Part Number: TUSB215 Other Parts Discussed in Thread: TUSB211 , Hi team,
There is an USB 2.0 with cable 5m design case.
In the datasheet, we see "Supports up to 5m pre-channel or 2m post-channel Cable Length".
What's the meaning for pre-channel…
Part Number: TUSB215 Is it possible to use an Trimpot for adjusting the Boost Levels for different applications? Or do the resistors have to be enabled via a micro controller?
Regards, Tim
Hi Takahashi-san,
YOSHIKAZU TAKAHASHI said: ■Can the combination of 4m pre-channel and 3m post-channel be applied to TUSB216?
Yes, this should be a setup where the TUSB216 would be applicable.
YOSHIKAZU TAKAHASHI said: ■I would like to use a 4m cable for…
Part Number: TUSB215 Hello
My customer want to develop USB 2.0 cable, and the length is 5m/10m/20m.
can we use TUSB215 to enhance the USB 2.0 signal for 5m, 10m, or 20m cable ?
How long of the cable does 1 piece of TUSB215 support?
If cable length is 5m…
Part Number: TUSB215 Dear Team
For the TUSB215 test in the datasheet, every time should power on(RSTN) to reset the device to have a test, so for a real application, the system will only power up one time and the TUSB215 will be reset. After that, the…
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/685426/tusb215-does-tusb215-support-bc1-2-in-slave-side
not sure whether it's true for TUSB216, similar scenario.
Part Number: TUSB215 Hi E2E team.
This is Jonathan from Avnet.
One of our customers, applied TUSB215 to CAR-Amp system in order to compensate for signal loss in a transmission channel.
In spite of that, they have not been able to pass the Apple ATS(Accessory…
Part Number: TUSB215 Other Parts Discussed in Thread: TUSB214 , TUSB213 , TUSB212 Hi team,
Do we have some suitable USB 2.0 redriver to recommend to improve the eye diagram performance?
i checked the esp and find the TUSB215 . Do you have more suggestions…
Hi Shirakawa-San,
Do you know the wire gauge? Please refer to the below table for the maximum pre-channel loss to pass and the maximum post-channel loss to pass. Since TUSB215 can support a maximum 8m with HIGH DC boost on the table, I think TUSB216…