Part Number: TUSB211A-Q1 Other Parts Discussed in Thread: TUSB216 , TUSB213 , TUSB212 Tool/software: Hi,
To perform USB end to end signal integrity, need IC SPICE/PSPICE models and other supporting documents.
Part Number: TUSB216I Other Parts Discussed in Thread: TUSB216-Q1 Hi expert,
My customer asked a question regarding EQ settings on TUSB216I.
I understood that Edgd/DC boost is helping maintain high/low voltages in the EYE pattern and RX sensitivity help…
Part Number: TUSB211 Other Parts Discussed in Thread: TUSB216-Q1 , , TUSB216 Hello TI experts,
my customer made Apple carplay module with TUSB211.
the problem is, newer iPhone (over iPhone 12) cannot connect to the car through carplay module. (under iPhone…
Part Number: TUSB212 Other Parts Discussed in Thread: TUSB216 , TUSB216-Q1 How much the maximum gain of the USB2.0 signal of TUSB 212? We want to make a USB2.0 10m extension cable, and plan to use one before and after the input and output respectively to…
Hi Chase,
I apologize I didn't know your question was posted and missed the response.
Please below the comments of the following customer's question from another thread . Note that it would be appreciated if you could tell the customer to ask any…
Part Number: TUSB214-Q1 Other Parts Discussed in Thread: TUSB216 , TUSB214 Eye Diagram test.
Even if the EQ and DC Boot settings are changed, the output results are the same. What Eye Diagram should I additionally check?
Hi Roy,
I recommend promoting the TUSB216-Q1 here as it is the same package a TUSB211-Q1. The Boost pin controls both AC boost (EQ) and DC boost (TUSB211-Q1 does not have DC boost, TUSB212-Q1 does). TUSB216-Q! and TUSB217-Q1 have stronger AC boost and…
Part Number: TUSB211 Other Parts Discussed in Thread: TUSB216 , TUSB216-Q1 Hi Team,
Here is a design scenario,
PCH to MB 5 inch > Cable 7 inch > daughter board 2 inch
Do you think TUSB211 have capability can support here?
Will suggest customer put…
Part Number: TUSB212 Other Parts Discussed in Thread: TUSB216-Q1 Hi Malik Barton57 ,
Thanks for the response. Can you please confirm what is the Maximum Pre channel and Post channel length supported by this TUSB212 Redriver .
Thanks
Hi Kura-San,
TUSB213-Q1 and TUSB217-Q1 can be and have been used in these applications. I recommend TUSB216-Q1 and TUSB217A-Q1 as they are improved versions of TUSB213-Q1/TUSB217-Q1. TUSB216-Q1 and TUSB217A-Q1 both support Android Auto and Carplay.
1) All…