Hi,
TUSB216I has some update for Eye diagram testing, TUSB216 and TUSB216I have the same performance outside compliance testing. I recommend using TUSB216I. I am not sure on MFI testing specifically, If customer is replacing TUSB217-Q1 with TUSB216-Q1…
Part Number: TUSB216 Hi, Support Team
It is reported that the customer has heard the news that the TUSB216-Q1 (Automotive product) will be released.
I searched through ti.com for the product, but there is no information, so I request the following information…
Part Number: TUSB216 Hi Team,
We would like to know about function of TUSB216
-edge boost along with DC boost
-RX sensitivity
-------
[Q1]
What is the effect of "edge boost along with DC boost" and "RX sensitivity" on USB eye pattern?…
Part Number: TUSB211 Other Parts Discussed in Thread: TUSB216 Hi,
A customer wants to use the TUSB216 as a replacement for the TUSB211.
I have received the following inquiries and request an answer.
- TUSB211 EQ
- TUSB216 BOOST LEVEL
Q1. Do EQ Level…
Part Number: TUSB213 Other Parts Discussed in Thread: TUSB217 , TUSB216 , TUSB217-Q1 My customer is looking to use TUSB213 as an alternative to TUSB217. The difference from a footprint perspective is the capacitor on VREG.
Their current design left this…
Hi Malik-san,
I would like to use TUSB216 x2pcs for 12m cable, so I have three questions.
--------
[Q1]
I understand that you recommend very good cable construction (large gauge cable).
Could you please let us know a recommended cable vendor(parts number…
Part Number: TUSB214-Q1 Other Parts Discussed in Thread: TUSB212-Q1 , TUSB216 We have an application that will be transmitting USB 2.0 over ~15ft and also in the presence of some power supply and motor noise (though the twisted pair with the USB signals…
Part Number: TUSB212-Q1 Other Parts Discussed in Thread: TUSB211 , TUSB212 , TUSB216 Hi
I am designing a system with a USB2.0 Host .
I wish to prototype with an option for a redriver, and since I should connect shorter than 0.5m cables (non standard) only…
Part Number: TUSB211-Q1 Other Parts Discussed in Thread: TUSB214-Q1 , TUSB214 , TUSB211 , TUSB217-Q1 , TUSB216 Hello team,
My customers ask some qustions if TUSB211-Q1 + TUSB214-Q1 can be used in their usb port for automotive application as diagram below…