Hi Allan,
I mentioned them for internal PU/PD value for TUSB216I. If you are asking about TUSB212, you can refer to the app note. (TUSB212 schematic checklist)
Best,
Josh
Hi Lumina,
As I mentioned above, TUSB211 might not match your expected cable length. Actually, the max distance would also depend on the USB data source drive strength and signal quality. In most cases, the 5m/3m case is the max distance with TUSB212…
Part Number: TUSB216-Q1 Other Parts Discussed in Thread: TUSB216I Hi Experts,
Seeking your assistance on this query from Cx:
For the TUSB216I USB 2.0 High-Speed Signal Conditioner with BC 1.2 Controller, I don't know what cable length my customer might…
Hi Shirakawa-San,
Do you know the wire gauge? Please refer to the below table for the maximum pre-channel loss to pass and the maximum post-channel loss to pass. Since TUSB215 can support a maximum 8m with HIGH DC boost on the table, I think TUSB216…
Hello,
The TUSB216I datasheet provides some more clarification on this:
If 0.75 V < VIN < 3.3 V when VCC is greater or equal to 4.5V, then RX_Sen will read a mid-level input.
When VCC < 4.5V, if 15% of VCC < VIN < 75% of VCC, then RX_Sen will read…
Hi Makoto-San,
After asking and looking around, it sounds like it would be best to try increasing the value of that resistor to 15KOhm. Going against the spec specified by the datasheet may lead to problems.
If you see any issues with your eyes/signals…
Part Number: TUSB217A-Q1 Other Parts Discussed in Thread: TUSB216I , TUSB217-Q1 Hi team,
I have couple of questions on TUSB21x family, i looked through the e2e history question but no clear answer:
1. RX pre-equalization for ISI compensation: can you give…