Part Number: TUSB8041 Other Parts Discussed in Thread: TUSB8044A , TUSB8040 Hi.
As you know if we install USB port, there's removable icon like as below.
Any possible to hide the removable icon if downstream has dedicate USB device?
Part Number: TUSB8041 Other Parts Discussed in Thread: TUSB8040 , Could you please share the EEPROM utility? I need to customize the status LED function for my design.
Other Parts Discussed in Thread: TUSB8040 , TUSB8040A1 , TPS2514A , TPS2513A , TPS2513 , TPS2511 , TPS2514 Hello,
I have question of TUSB8040.
When I use TUSB8040 as DCP only, Is the USB controller not necessary?
When I use TUSB8040 as DCP only, What kind of…
Other Parts Discussed in Thread: TUSB8040 , TPS74801 , TUSB8040A , PCM2903C Hello!
I am actually trying to build an USB3.0 hub with the TUSB8040 Chip.
The problem is that is not working. I tried to build it very similar to the schematic of the evaluation…
Other Parts Discussed in Thread: TUSB8040 We have a design with a built in USB3.0 hub using TUSB8040. Once a USB3.0 device were recognized as USB2.0 because of a cable fault. After changing the cable, the problem wasn't solved.
We could only solve…
Other Parts Discussed in Thread: TUSB8040 Since USB 3.0 is dual simplex, is the TUSB8040 able to access two devices concurrently? For example out to device one on the output simplex pair and in from device two on the input simplex pair.
Thanks,
DFAE
Other Parts Discussed in Thread: TUSB8040 In the data sheet, supply current is said to be 460mA/VDD11 and 135mA/VDD33, or a total of about 0,95W when running high speed US-connection and no DS connections. When trying the TUSB8040, both on the eval-board…
Other Parts Discussed in Thread: TUSB8040 Hi,
I made a TUSB8040 board and routed the super speed signal pins only (both the upstream and downstream links).
Now the board could not be recognized by the computer, and the "SS" and "HS_SUSPENDED" LEDs were…