Part Number: TUSB8042A HI Teams When only USB 2.0 is supported in the downstream port, How should unused SSTX_P/M and SSRX_P/M pins be handled? Please.
Part Number: TUSB8042A Hi,
Can you help to answer a question I have regarding valid combinations of the USED[3:0] bits. Table 15 indicates that both ports 1 and 3 cannot be marked as disabled. While the 5 th line in table 5 shows and example where ports…
Part Number: TUSB8042A Other Parts Discussed in Thread: TUSB8041 , TUSB8041A , TUSB8042 , Hello guys,
One of my customers is considering using one of USB8041, 8041A, 8042 or 8042A for their new products. They want to use the device as 5Gbps 4 port USB3.0 HUB…
Part Number: TUSB8042A The maximum ratings of the XI are given in the data sheet. (see below) What is the input voltage VIL(max) and VIh(min) of the XI? I am currently considering connecting an oscillator with a 1.8 V output. The output provisions are as…
Part Number: TUSB8042A Dear team,
Is the I2C communication able to operate at 1.8V?
From datasheet: The external interface is enabled when both the SCL/SMBCLK and SDA/SMBDAT pins are pulled up to 3.3 V at the de-assertion of reset.
From this I would assume…
Part Number: TUSB8042A Other Parts Discussed in Thread: TUSB8041A , , TUSB8041 , TUSB8041EVM , TUSB8042 Dear tech consultant
We received the circuit diagram for the TUSB8041A chip from TI and also purchased the reference board (TUSB8041AEVM).
And with the…
Part Number: TUSB8042A Other Parts Discussed in Thread: TUSB8020B , , TUSB8044A , TUSB8043A Can you confirm that the "A 1.05-V, 1.1-V, or 1.2-V supply may be used as long as minimum and maximum supply conditions are met." statement for the VDD power rail…