Part Number: TUSB8042A Hi
Want to know what is the difference between the two functions under the USB Hub IC?
1. HID programming interface
2. USB 2.0 Billboard support
Conditions: Input signal USB3.2 (10Gbps), convert to two or four USB3.2 (5/10Gbps…
Part Number: TUSB8042A hello.
Our board has a processor and a TUSB8042A, which is connected to the upstream side of the TUSB8042A via a USB 2.0 interface. However, in the case of on-board connections, the EYE mask rule of the USB 2.0 standard does not…
Part Number: TUSB8042A Other Parts Discussed in Thread: TUSB8042 Hi,
We are using TUSB8042 can we have eeprom programming tool along with documentation.
Thanks!
Jeff
Part Number: TUSB8042A Other Parts Discussed in Thread: TUSB8044A Hi support team,
Are there any IBIS models for TUSB8042A ? I'd like to simulate TX and RX lines using keysight ADS.
Sincerely
Part Number: TUSB8042A Other Parts Discussed in Thread: TUSB8042 Hello.
In our circuit, after the TUSB8042A is powered up, the config setting is executed from the HOST via the SMBUS interface. The hard configuration setting pin of TUSB8042A is set as follows…
Part Number: TUSB8042A Hi Team,
I am supporting a USB3.x design - and there are some generic routing questions I am trying to answer. I am referencing this literature for design info: https://www.ti.com/lit/an/spraar7i/spraar7i.pdf In a multi-layer board…
Part Number: TUSB8042A Hello. Previously, we used one TUSB8042A Device to check the operation, and this time, we are going to check the operation using two devices. I am writing because I have a question about clock input during the circuit configuration…
Part Number: TUSB8042A Hi team,
I look for a solution to debug my system with USB interface.
I need a USB HOST IC to send "SET POET FEATURE (PORT POWER)" command to the USB HUB IC through USB cable.
This is just debugging purpose and no other…
Part Number: TUSB8042A Other Parts Discussed in Thread: TUSB8043A
Hello,
We have an application in which we use TUSB8042A/43A. We have three USB 3.0 type-A downstream ports (ports 1 to 3) which are removable and one non-removable USB 2.0 downstream…