Part Number: TUSB8043A Hello Team,
We are using TUSB8043A USB HUB in our design. Our application we are using 4 port as below configuration.
USB 1 : USB TYPE C HOST
USB 2 : USB TYPE A HOST (Expansion Header)
USB 3 : USB TYPE A HOST (Expansion Header) …
Part Number: TUSB8043A Dear Sir:
From TUSB8043A ds: "The TUSB8043A provides pin strap configuration for some features including battery charging support,
and also provides customization though OTP ROM, I2C EEPROM, or via an I2C/SMBus slave interface…
Part Number: TUSB8043A Hi Support Team,
in the data sheet in section 11 / Layout there is a remark:
11.1.3 - 11: To ease routing, the polarity of the SS differential pairs can be swapped. This means that SSTXP can be routed to SSTXM or SSRXM can be routed…
Part Number: TUSB8043A Hi TI Teams,
Our customer reported that when TUSB8043A is connected to two USB2.0 Cameras and is doing streaming at the same time, but found that only one of the two cameras can be used for streaming, and the other cannot. They checked…
Part Number: TUSB8043A Other Parts Discussed in Thread: TUSB8044AEVM Could I please get access to the Windows EEPROM Programming Tool mentioned on page 4 of the TUSB8044AEVM User's guide?
Part Number: TUSB8043A Other Parts Discussed in Thread: TPS2595 Hi Team,
We are finalizing one hardware design with TUSB8043A and Jetson Nano SOM. We would like to get the same reviewed by TI community, block diagram attached Requirements: 4 Port USB…
Part Number: TUSB8043A Hi Team,
My customer is looking for USB Hub for USB3.1 Gen1 (5Gbps) device, however the host will connect to USB3.1 Gen2 (10Gbps).
block diagram is like below, customer is asking if TUSB8043A can be recognized from USB3.1 Gen2…
Part Number: TUSB8043A I have tested USB3.2 undernal the following conditions,
But no test signal is output.
1:The DTU is turned on, If the DTU is peripheral, Vbus is supplied from the USB connector.
2:There is a tceduermination (50OHM) on the Tx line…
Hello Xiaobo,
Yes, the end result would be the same from both traces but the protocol looks a bit different, the trace that shows the warm reset doesn't show any errors before that just an entry to U1. U1/U2 is definitely still enabled in this system…