Part Number: TUSB8044 Goodmorning, if i want to avoid using the eeprom and any other smbus, i2c communication protocol, which is the I/O configuration to adopt?
I saw the evaluation board, but there are the dip switches on the board, and it is not specify…
Part Number: TUSB8044 Hi Team,
My customer would like to know about clock input.
Regarding the clock input, is there a specification of the minimum value maximum value of VH and VL?
The clock oscillator that my customers want to use is as follows.
Can…
Part Number: TUSB8044 Hi Team, Is it possible to apply USB_VBUS before VDD and VDD33 is off (=GND)? I believe it is possible however would like to confirm just in case.
Best Regards, Yaita
Part Number: TUSB8044 Hi
I have some question about TUSB8044 EEPROM Data
1. Some BYTE ADDRESS are Reserved. How should I set these address? All 0b, all 1b or don't care?
2. BYTE ADDRESS 100h-2DF are "USB Billboard Strings 1 and 2". How should…
Part Number: TUSB8044 Dear sir,
Our customer is using TUSB8044, and they want to ask a question.
Because this project is ARM based, not Windows based.
They want to confirm that is TUSB8044 suitable for the testing methodology as attachment for USB2.0…
Part Number: TUSB8044 Hello
if customer would like implement USB to I2C tool via TUSB8044, they could use USB to update firmware to main chip. Has any driver requirement of TUSB8044 for this feature implement? If yes, please help provide driver or…
Part Number: TUSB8044 Hi Team,
I would like to know.My customers are considering using TUSB8044.
If Host is a USB 2.0 only compatible product, is it possible to use TUSB8044 for UPSTREAM PORT?
What should I do with 'USB_SSxXx_DNx' pin processing when…
Part Number: TUSB8044
Hello there,
I'm trying to use the TUSB8044 with a TPS65987D as the PD Controller, but I'm having some issues figuring out the Billboard related pin's connections. On the TUSB8044 datasheet, it mentions that the PD controller…