Part Number: TUSB8044 Hi,
I received below question from my customer.
When TUSB8044 is connected with USB3.0 Host and USB 3.1 device, does communication success?
I think that it can success because these devices recognize each other by enumeration.
Is…
Part Number: TUSB8044 Hi,
I use TUSB8044 in I2C mode. I'd like to use pin 42 as BBEN.
When pull-up the pin 42 with 10K, the voltage become 1.8V.
Does the pin42 have internal 12K pull-down?
Would you tell me the internal equivalent circuit of pin 42? …
Part Number: TUSB8044 Other Parts Discussed in Thread: TUSB8041-Q1 Hi team,
Customer requires one SD interface and two USB interface when use automotive HUB device, could you please help to check and provide the whole solution? Thanks!
Best Regards
Zhengquan…
Part Number: TUSB8044 Hi
Please clarify the statement from TUSB8044 datasheet :
"When the upstream port is connected to an electrical environment that only supports high-speed or full-speed/low-speed connections, SuperSpeed USB connectivity is disabled…
Part Number: TUSB8044 Other Parts Discussed in Thread: TUSB7340 Hi,
an engineer is designing a hub with TUSB8044 and is asking if we have the USB SS pinout of a USB Host?
Thank you!
-Alberto
Part Number: TUSB8044 Other Parts Discussed in Thread: TUSB8040 Hi guys,
My customer is using the TUSB8044 in a design and they are having a hard time with the EEPROM:
We have a current requirement for 4-port Superspeed USB hub, so I am evaluating the…
Part Number: TUSB8044 Hi,
Can I get the software to be able to program the EEPROM over USB?
Also, does a default config file for the EEPROM exist? It would be helpful.
Thanks
Part Number: TUSB8044
Dear TI engineer
I want to know the minimun of "HIGH level input voltage" and the Maximum of "LOW level input voltage".
Would you tell me about following input Pin?
1. USB_VBUS
Best Regards
Part Number: TUSB8044 Other Parts Discussed in Thread: TIDA-01243 , , TUSB8041 , HD3SS460 Hello Team,
I have a few questions about the differences between an MST HUB and a USB HUB. I am creating a dock block diagram for us to use here in the field. It's…