Part Number: TUSB8044 Other Parts Discussed in Thread: TUSB8043 Hello
I want to ask, TI USB3.1 Hub has the following specifications of the plan?
Upstream Port
1x USB3.1 Gen1
Downstream Port
3x USB3.1 Gen1
Power Charging Port
1x Charging Port required…
Hi Gregor,
Yes, I used a full-speed hub.
All the high-speed hubs are TUSB804x or TUSB802x, the full-speed hub is the Belkin FSU101. Belkin ExpressBus (F5U101) 4-Ports External Hub for sale online | eBay
If it helps raise your confidence in the TUSB8044…
Part Number: TUSB8044A Other Parts Discussed in Thread: TUSB8044 Dear team,
1. At datasheet, I2C speed is 100K and 400K(default) and then, How about SMBus speed? Is it same with I2C speed?
Please let me know maximum speed of SMBus interface.
2. After…
(fat fingered early submit of incomplete reply) The TI database shows TUSB8044EVM for TUSB8042 and TUSB8043.
Is TUSB8044 also similarly interchangable on a PCB as TUSB8042 and TUSB8043?
How different is code developed on TUSB8044EVM for TUSB8042 and…
Part Number: TUSB8044 Other Parts Discussed in Thread: TPS2546 , When the upstream port is connected, can one downstream facing port be switched into DCP mode? Other 3 ports continue to be used as SDP.
A customer is using a usb hub and one downstream facing…
Part Number: TUSB8044 Hello,
I am designing a USB based hub and I have chosen the TUSB8044 for the USB - hub/Billboard implementation. However I did not find enough resources for its Firmware or any code that runs on the system.
Please let me know if…
Part Number: TUSB8044A Other Parts Discussed in Thread: TUSB8044 Hi,
We are doing jetson SI test, using jetpact version 5.0.2.
linux kernel version 5.10.104
ubuntu version 20.04.4 LTS
What should the TUSB8044 register set during SI test?
There is any command…
Part Number: TUSB8044A Other Parts Discussed in Thread: TUSB211 , TUSB8044 Hi,
My customer use TUSB211 USB 2 redriver in front of TUSB8044A.
At specific NB upstream + cable + downstream camera. NB will disconnect the hub sometimes after showing the camera…
Part Number: TUSB8042A Other Parts Discussed in Thread: TUSB8044 Hi Team,
Customer is asking for TUSB8042A EVM layout file in Orcad (BRD).
I guess we only have TUSB8044 EVM that can be referenced, correct me if I am wrong.
Also can someone please send …
Part Number: TUSB8041 Other Parts Discussed in Thread: TUSB8044A , , TUSB8020B , TUSB8042A , TUSB8044 , TUSB8042 , TUSB8043 , TUSB8040 , TUSB8043A
USB 2.0 high speed signal quality (eye diagram) testing requires a USB port to send a USB 2.0 test packet. All USB…