Part Number: TMDXEVM8148
Hi Everyone,
I'm trying to hook up the tvp5147 with the v4l2 capture driver and now i have an issue with i2c:
tvp514x 1-005c: Write: retry --- 0 tvp514x 1-005c: Write: retry --- 1 tvp514x 1-005c: Write: retry --- 2 tvp514x 1…
Part Number: TVP5147EVM
Hello,
Is there a more updated version of the TVP5147 EVM board?
I would like a board which converts an analog video input to any type of digital video format (with pin interface to connect it to another board.)
The final goal is…
Other Parts Discussed in Thread: OMAP-L138 I'm trying to capture video from analog cam, connected to OMAP-L138 LCDK via composite-in. When I'm executing vpif application as vpif_mmap_loopback -m 1 -p 0 the following error appears
______________…
Other Parts Discussed in Thread: TVP5147 I am working on capture from TVP5147 on TI8148 EVM.
I have tried with hdvpss package by adding device setting for TVP5147 and modifying captureVip example but in output only getting green frames.
Then I have tried…
Hi margarita,
Thanks for your helpful reply.
After using "filesrc location=..." resolution is coming correctly but not for capture and display using "omx_camera".
I can't use "v4l2src" because presently I don't have v4l2 driver for…
Other Parts Discussed in Thread: TVP5147 Hi All
We are working on a custom board based on DM8168. We are using EZSDK(ti-ezsdk_dm816x-evm_5_05_02_00).
We have connected TVP5147 on VIP1 of DM8168 and configured it in 20bit 4:2:2 discrete sync mode. After…
Other Parts Discussed in Thread: TVP5147 , SYSBIOS
We are trying to get video for processing from TVP5147.
Following are our observations based on the tests and inputs on ti forum:-
1 – We have checked the TI diagnostics package and the results are as…