See attachments for additinal customer inputs ('section 3' portion of inquiry, below, refers to the 'DS2200 ... Word attachment).
***************************************************************************************
We are half way thru…
Other Parts Discussed in Thread: TVP70025I Hello TI Experts,
I have a system using a DM368, with video capture coming from a YUV source (component input attached to a TVP70025i). I am using the resizer to convert this input into YUV420SP, as required by…
Hello Michael,
The coarse offset refers to an analog offset implemented before the ADC.
The fine offset refers to a digital offset implemented after the ADC.
The TVP70025i includes an automatic level control (ALC) algorithm to control the fine digital…
Hi,
Is this an RGB component format? The TVP7002 (0C-70C) or TVP70025i (-40C - 85C) triple ADCs may be the best fit for support of RGB component formats. The TVP51xx video decoders target only 525-line and 625-line formats. It appears that there may be…
I wanted to have as a input (1280 x 720) VGA and have the kit convert this to 720p component video. The preset resolutions that the kit comes with does not have a setting for (1280 x 720) but is has a setting for (1280 x 768). So I downloaded the tvp7002_ths8200_evm_kit_081811…
Other Parts Discussed in Thread: TVP7002 Per datasheet the TVP7002 wants 1.9V for its core voltage verses the TVP70025 which specifies 1.8V. I know the 70025 is specified for industrial temperatures and cost more. The TVP7002 can digitize at higher frequencies…
Other Parts Discussed in Thread: TVP7002 Hi all:
We are making our own dm365/dm368 board, which has s-vedio, composite, component & VGA input. when capturing VGA video which at XGA@60Hz, there are some problems:
1. the vertical alignment…