Hi Shiven,
That is correct, and even if we have TVS1800 in series back2back with forward voltage of min. 0.25V that is still 34.25V.in worst case.
Although I have never used TINA TI, now I made a rapid learning to put up a simple simulation with load…
Hi Inho,
You can also order TVS1800 samples from ti.com
https://www.ti.com/store/ti/en/p/product/?p=TVS1800DRVR
This part is currently out of stock, but we are in the process of replenishing stock. You should be able to order by next week, or by…
Part Number: TPD1E10B06 Other Parts Discussed in Thread: TPS25947 , TPS25947EVM , TVS1801 , TVS1800 , TVS2200 Hi, TI expert
The customer company has a question about selecting a TVS device with a surge function.
Q1) Can I confirm what level the TPD1E10B06…
Other Parts Discussed in Thread: TVS1800 , LM5069
Hello,
at the time we connect our device to the battery, a spark (because of a high inrush current) on the battery connector is heard and visible. So, I'm looking for a reliable high side N-MOS driver…
The IC is burned and then there are no issues on other boards which use the same IC. All other boards are working fine.
The switch over of this IC was proper when it was alive, and when the burning happened, there was no switch over, but it was working…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…
Part Number: TVS2700 Other Parts Discussed in Thread: FLAT-CLAMP-TVS-EVM
One of my customers was recently looking for TVS diodes to protect their system from surge events, and they came across TI's TVS flat-clamp devices, particularly the TVS2700. They…
Part Number: LM74700-Q1 Hello,
I have two questions related to Fig. 21 in LM74700-Q1 datasheet.
1. The recommended TVS+ is SMBJ58A, with the breakdown voltage of 64.4-V (minimum), 67.8 (typical). It it were connected to the ground alone, it meets…
Part Number: TVS1400 Other Parts Discussed in Thread: TVS0500 , TVS0701 , Hi,
In my earlier post i had raised the below query
Planning to use TVS1400 on 12V DC line and TVS0500 on 6.2V DC Line. Since on TVS0500 VRWM is 5V, but the Clamping voltage…