Part Number: TXB0106 Other Parts Discussed in Thread: TXU0202 Dear TI team, Could you please let me know whether TXB0106 can be used for UART interface? Below are my requirements for the design. VCCA: 1.2V VCCB: 3.3V Speed: 115200 Regards Shyam
Part Number: TXB0106-Q1 Hello,
I am writing to make sure that my planned use of the TXB0106-Q1 as a 5.0V->3.3V level shifter will work. I intend to drive an attenuator that requires 6 3.3V control signals with our hardware driver that uses 5.0V logic…
Part Number: TXB0106-Q1 Hello,
I am using the TXB0106-Q1 to level shift a number of logic pins from 5.0 to 3.3v, and due to the # of pins not being a multiple of 6, i have some leftovers on the last level shift IC. Schematic of this IC attached below…
Part Number: TXB0106 Other Parts Discussed in Thread: TXU0104 , TXU0102 , Hi,
I am using TXB0106PWR for converting 3.3v to 5.V logic levels, facing challange in getting clean output
all signals are uni directional o/p of 3.3V microcontroller system…
Part Number: TXB0106 Hello,
The datasheet states that if VCCA and/or VCCB is unpowered, the pins of the corresponding port are placed in a high-impedance (tri-state) mode to prevent current drain.
If Vccb=0 and Vcca=1.8V, what are the state of port…
Part Number: TXB0106 Other Parts Discussed in Thread: TXU0102 , TXB0104 , TXB0304 Tool/software:
Currently, we are designing a QSPI interface between a system controller (1.5V) and a flash device (1.8V), and we have selected the TXB0106 for voltage…
Part Number: TXB0106 Tool/software: Is there an Adapter / TestSocket vor this IC ??? We need to test and preselect every batch which is delivered to us because some batches working fine, some working with 50 percent failure.
Part Number: TXB0106-Q1 Hi Team,
Hope you are doing good !!
We have received a new part request for the 'MPN: TXB0106QWBQBRQ1 NewPartQuestionnaire_TI_TXB0106QWBQBRQ1.xlsx ' which is requested for the project 'ADAS'. I have attached the questionnaire…
Part Number: TXB0106 Hello,
We have an application where we are running RS232 and RS485 signals through the TXB0106RGYR to level shift between 2.5V and 3.3V. It is unidirectional, but the bidirectional TXB0106RGYR has been picked to combine 5 signals…
Part Number: TXB0106 Other Parts Discussed in Thread: TXU0204 , TXU0101 Hello,
We have an application where we are running RS232 and RS485 signals through the TXB0106RGYR to level shift between 2.5V and 3.3V. It is unidirectional, but the bidirectional…