Part Number: TXB0108 Other Parts Discussed in Thread: TXS0102 , LSF0102 , TXU0104 Hi
My customer explained to me the application situation:
The A side is connected to the GPIO.
The B side is connected to the Ethernet chip.
The signal is I2C, and is the…
Part Number: TXB0108
Hi, Support Team
We find the clock/data signal before STOP signal have a signal(orange block), what is mean?
as below chart:
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TXB0108 Other Parts Discussed in Thread: TXU0104 Hi~
Can you please help me review this schematic and peripheral devices' parameters? According to my understanding, this schematic is out of problem~
If you have any other problems or concern…
Hey Godziller,
I see, thanks for clarifying. Taking a closer look at the FETs that are being driven, it seems the input capacitance is above what the TXB0108 can drive (max loading conditions is 70pF):
You may need to resort to fixed direction translators…
Part Number: TXB0108 Hello everyone. I have an interesting issue that I am currently working on. What I am seeing for the output of my circuit is that the outputs are all half-logic. I have been trying different things such as reflowing the chip but it…
Part Number: TXB0108 Other Parts Discussed in Thread: TXB0104-Q1 Hi,
I found TXB0108 Driving current is not enough for my application.
I found TXB0104-Q1 seems can support to 40uA.
Do you have any better suggestion?
Thanks!
Jeff
Part Number: TXB0108 Other Parts Discussed in Thread: TXU0104 , TXU0204 , One of our circuits uses the level conversion chip of your company TXB0108DQSR. The load device is the scanner dock (3.3V), and the control signal is output by the CPU (1.8v). The…
Part Number: TXB0108 Other Parts Discussed in Thread: TXB0304 , TXB0104 Hi team,
My customer is using our TXB0108PWR now.
And in a new project, they need a 200MHz data rate.
Could you please kindly help check if we have a p2p device with a 200MHz data rate…
Part Number: TXB0108 Other Parts Discussed in Thread: TXU0104 , TXS0108E Hi,
We used TXB0108 in between MCU (3V3 CMOS logic) and LCD ( 5VTTL logic), we faced issue with LCD function not for all but some LCD characters not displayed .
1. Can we use TXB0108…