Part Number: TXS0104E Dear TI experts,
My customer tests their own PCB which is used TXS0104ERTUR.
In the test they found that if OE is low, all outputs are high-impedance state, it is mentioned on the datasheet.
But actual measurement value is…
Part Number: TXS0104E Other Parts Discussed in Thread: TCA9800 Tool/software: Hi team,
Customer has used TXS0104E to transfer I2C signal, but has found that the low level is not near 0V. Is there any clamp voltage in the internal leading to this issue…
Part Number: TXS0104E Hello! I've been using the TXS0104EPWR in a design and recently received a batch of boards from a contract manufacturer and these parts are non-functional on those boards. I noticed the part markings appear to be dramatically different…
Part Number: TXS0104E we have been using the TXS0104EPWR for a while, but the latest lot as some issues on our i2C with the touch screen not working correctly... only differnece is the lot/batch number on the device.
is this a known thing between lots…
Part Number: TXS0104E Sehr geerhte Damen und Herren,
wir haben die Artikel mit der HTN TXS0104ERGYR und HD3SS3220IRNHR bei uns in Verwendung.
Bei der Wareneingangsprüfung ist nun aufgefallen, dass die Bauteile laut Datenblatt und Homepage den MS-Level…
Part Number: TXS0104E Other Parts Discussed in Thread: TCA9803 Tool/software: Hi team,
I would like to ask that if TXS0104E can support the I2C and I3C protocol since it has the Open Drain integrated resistor? I assumed that it could work as long…
Part Number: TXS0104E Hi Team,
I am supporting a customer who is using the TXS0104EPWR. Both VCCA and VCCB are connected to the same 3.3V power supply.
They are experiencing an issue where a voltage spike/glitch occurs on the rising edge of the signal…
Part Number: TXS0104E I would like to use TXS0104EPWR in MDIO line.
TI website recommends use for MDIO.
However, MDIO standard class 45
When VDD is 1.8 V, VIH (min) is about 1.26 V
VOL (max) is about 0.36 V.
On the other hand, TXS0104 data sheet…
Part Number: TXS0104E Hi team,
I'm using the level translator TXS0104EQPWRQ1 in my board.
Please confirm whether unused inputs and outputs can be made as NC or any termination required.
Regards,
Abhishek