Part Number: TXS02326A Tool/software: Hi, please, i need to know more about the BSI, OE and SDN pin's. Can you help me with any explanation? And if possible some schematics examples using the device.
I'm eletronic engineer and i'm working in a solution…
Part Number: TXS02326A Tool/software: I want to run these two chips in parallel with 1 modem so I can utilize 4 outputs. Is there an EN function so that I can disable one of the IC's when I am multiplexing?
Part Number: TXS02326A Other Parts Discussed in Thread: TMUX1574 , TXS4558 Tool/software: Hello,
My customer is looking for an analog switch IC with the following features;
Please recommend a suitable product among TI products.
Thank you.
J…
Part Number: TXS02326A
Hi Team,
Can you please help us with our customer's inquiry below?
I am making a design with 2 sims, specifically a physical sim and an e-sim. We are working with the Compute Module 4 of Raspberry Pi and its I/O Board. To…
Part Number: TXS02326A I'm trying to understand if my application will benefit in any way from the external clock. I understand that an external clock can offer higher stability, precision, and the ability to sync multiple devices. It looks like this…
Part Number: TXS02326A Hi
1. We do not use BSI input of TXS02326A.
Can we leave the BSI input open or we must it pull up or pull down if "BSI detection behavior" bit is 1 in register 0Eh?
2. IRQ is used to set the I2C address.
Is the IRQ signal…
The i2cdetect utility starts a transaction and looks for the ACK, without actually reading or writing.
If the capacitive load on the I²C lines is too high (check for proper rising edges with an oscilloscope), reducing the pull-up resistors would help…
Part Number: TXS02326A Other Parts Discussed in Thread: TXS4558 Hi Team,
My customer needs to know what difference between txs02326A and txs4558.
could you provide comparison table and introduction slide.
Thanks
Part Number: TXS02326A Hello
The "SETTING UP THE SIM INTERFACE" section of the TXS02326A datasheet describes how to start the SIM interface.
In item 3 of the sequence is writen: "The baseband SIM interface is set to a LOW state."
Ours baseband is…
Part Number: TXS02326A Hi Sir,
Here are two Switching between SIM cards processes questions need your help.
1. How to put SIMx card interface into "clock stop" mode?
2. There are two scenarios when switching to SIM2 card are described on the datasheet…