Part Number: TXS4558 Hello,
Regarding to VSEL2 timing on TXS4558, my customer is asking some question.
In their application, VSEL2 is high during VCC is power up.
In this case, VSIM is output 2.95V correctly.
(Please refer bellow diabrames.)
(Question…
Part Number: TXS4558 Hello,
Regarding to VSIM* Start-up time(TSTR) on TXS4558, my customer is asking a question.
(Question)
・Which is start point of TSTR ?
Is it CSELsignal edge point? or VSEL* signal edge point?
Or is it from a point(ex.10%) to a point…
Part Number: TXS4558 Hello,
Regarding to SIM*I/O at deactivation on TXS4558, my customer is asking some question.
At deactivation(VSIM=1.8V), short pulse (about 1ms) is occurred after SIM*I/O is off.
(Please refer attached file.)
(Question)
(1) is this…
Part Number: TXS4558 Hello,
Regarding to input transition rise or fall rate on TXS4558 , my customer is asking a question.
(Question)
When Δt/Δ is more than 5ns/V, is there any impact on this device?
It will be about 20ns/V on their application…
Part Number: TXS4558 Other Parts Discussed in Thread: TXS0102 Hello,
Regarding to VSIM* and SIM*I/O on TXS4558, my customer is asking some question.
(Question)
1)When EN*=H and Vcc=0, is VISM* off?
2) Do you have a data of VIL/VIH in SIM*I/O?
Regards…
Part Number: TXS4558 Hello,
Regarding to TXS4558, my customer is asking some question.
(Question)
(1)For power up, is power sequence is needed?
Or don’t we need to care power procedure ? (VCC and VBATT)
(2)VBATT is always input to power source…
Part Number: TXS4558 Dear Specislists,
My customer is considering TXS4558 and has questions.
I would be grateful if you could advise.
---
1. What is the device internal input protection circuit for each control pin (EN1 / 2, VSEL1 / 2, CLKRUN1 / 2, CSEL…
Part Number: TXS4558 Hi,
I am looking for 1 to 8 port sim card switch solution, may I ask that can we implement this by using this part?
What will also need in the system?
Please let me know if there are suggestion.
Thanks for your help.
Hi,
We are closing this post due to inactivity. Please feel free to post again if you have any other questions. We now have a goal of responding within 24 hours to any new post.
Regards,
Emrys