Part Number: TXV0106 Other Parts Discussed in Thread: TXV0108 Tool/software: Hello.
As written in the title, I would like to request a review because it appears to be an error in the data sheet. (descriptions that has a fixed direction but is treated…
Part Number: TXV0106 In addition to the error with the diagram on the first page of the datasheet, we have also found the following potential sources of confusion:
1. Figure 7-1 Functional Block Diagram of the TXV0106 shows an active high OE pin, as well…
Part Number: TXV0106-Q1 Tool/software: Hello team:
I have some questions about the output channel-to-channel skew and duty cycle variation described in the datasheet:
1. How are these two parameters measured, and what methods are used to obtain the values…
Part Number: TXV0106 Other Parts Discussed in Thread: TXV0108-Q1
Hello Team,
shouldn't Vcca and Vccb be switched for the lower part as this is a unidirectional level shifter?
Also Vout(min) should be corrected to 1.14V in the search parameters, right…
Part Number: TXV0106 Hi, our application will be translating an RGMII 1 GbE interface from 1.2V to 1.8V. I see a statement in the datasheet that says the following:
Does this mean an RGMII 250 Mbps line rate (for 1 GbE) can not be achieved in our application…
Part Number: TXV0106-Q1 Other Parts Discussed in Thread: TXV0106 Hi Team,
We are designing TXV0106 in RGMII and want to double check if this device can support 150mm trace length.
We know there are some parameter will impact the result, but in general…
Part Number: TXV0106 Hello Team,
the data sheet does not provide the following information:
1. channel to channel skew for Vcca = 1.2V?
2. switching characteristics for Vcca=3.3V and Vccb=1.2V?
May I ask you to provide this missing important information…
Part Number: TXV0106-Q1 Hello, I wanted to confirm the max data rate for this part? In one location you say max data rate of up to 500Mbps for 1.65 to 3.6V. In another you say 250Mbps/channel for RGMII 2.0.
Can you please confirm this port supports 250Mbps…
Part Number: TXV0106-Q1 Other Parts Discussed in Thread: SN74AVC2T45-Q1 , Please provide IBIS model and project details as follows
Device name of the model you are requesting :
SN74AVC2T45-Q1
TXV0106-Q1
Project details :
For simulating a 100Mbps application…