Part Number: LSF0204D Other Parts Discussed in Thread: TXU0104 , TXV0106 Tool/software: Hi,
Greetings...
We are planning to use LSF0204D in our application to translate a push-pull interface from 3.3V to 5V & vice versa. In the datasheet, related…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74AVC8T245 , DP83TG720R-Q1 , TXV0106-Q1 , TXV0106
Hi,
I am using DP83TG720R-Q1 1000BASE-T1 Automotive Ethernet PHY. This will be connected to ZU-7 SoC from AMD. The I/O voltage supported by SoC…
Hi Ganesh,
Yes, the datasheet specifies up to 100 MHz for 1.8 V outputs.
You may also see TXV0106 for an easier implementation, thanks.
Best Regards,
Michael.
Hi Imelda,
Please help see the TXU family (TXU0104-Q1 / TXU0304-Q1) or TXV0106-Q1 as our fastest Tr device as of this time.
You may also try using active probes (and avoid connectors) with little or less capacitance with the device's EVM so as to help…
Part Number: SN74LV6T17 Other Parts Discussed in Thread: TXV0106 Hello team,
Can I input 1.8V to the input pins, when the device is powered OFF?
I see, there is no clamp diode from input to Vcc, so I am assuming its okay.
Best Regards, Kei Kuwahara
Hi All,
Please see the new TXV level-shifter family (TXV0106-Q1 / TXV0108-Q1) supporting high-bandwidth timing-margin sensitive interfaces such as RGMII.
For more information, see Enabling high performance interface translation | Video | TI.com , thanks…